BeamSectionOffsetOptions Class¶
-
class
NXOpen.CAE.
BeamSectionOffsetOptions
¶ Bases:
NXOpen.TransientObject
To create a new instance of this class, use
NXOpen.CAE.CaePart.NewBeamSectionOffsetOptions()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AftOffset | Returns or sets the aft offsets |
ForeOffset | Returns or sets the fore offsets |
IsOffsetSpecified | Returns or sets the flag indicating whether the offset is specified |
OffsetMethodType | Returns or sets the method to define beam end offsets |
SameEndOffsets | Returns or sets the flag indicating whether the offset on both fore end and aft end are consistent |
Enumerations¶
BeamSectionOffsetOptionsMethod Enumeration | Represents the offset definition method |
Structs¶
BeamSectionOffsetOptionsOffset_Struct Struct | Represents the offset value |
Property Detail¶
AftOffset¶
-
BeamSectionOffsetOptions.
AftOffset
¶ Returns or sets the aft offsets
-------------------------------------
Getter Method
Signature
AftOffset()
Returns: Return type: NXOpen.CAE.BeamSectionOffsetOptionsOffset_Struct
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AftOffset(aftOffsets)
Parameters: aftOffsets ( NXOpen.CAE.BeamSectionOffsetOptionsOffset_Struct
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ForeOffset¶
-
BeamSectionOffsetOptions.
ForeOffset
¶ Returns or sets the fore offsets
-------------------------------------
Getter Method
Signature
ForeOffset()
Returns: Return type: NXOpen.CAE.BeamSectionOffsetOptionsOffset_Struct
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ForeOffset(foreOffsets)
Parameters: foreOffsets ( NXOpen.CAE.BeamSectionOffsetOptionsOffset_Struct
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsOffsetSpecified¶
-
BeamSectionOffsetOptions.
IsOffsetSpecified
¶ Returns or sets the flag indicating whether the offset is specified
-------------------------------------
Getter Method
Signature
IsOffsetSpecified()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsOffsetSpecified(isOffsetSpecified)
Parameters: isOffsetSpecified (bool) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
OffsetMethodType¶
-
BeamSectionOffsetOptions.
OffsetMethodType
¶ Returns or sets the method to define beam end offsets
-------------------------------------
Getter Method
Signature
OffsetMethodType()
Returns: Return type: NXOpen.CAE.BeamSectionOffsetOptionsMethod
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetMethodType(method)
Parameters: method ( NXOpen.CAE.BeamSectionOffsetOptionsMethod
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SameEndOffsets¶
-
BeamSectionOffsetOptions.
SameEndOffsets
¶ Returns or sets the flag indicating whether the offset on both fore end and aft end are consistent
-------------------------------------
Getter Method
Signature
SameEndOffsets()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SameEndOffsets(isSameEndOffsets)
Parameters: isSameEndOffsets (bool) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)