BeamSectionOffsetOptionsMethod Enumeration

NXOpen.CAE.BeamSectionOffsetOptions.Method is an alias for NXOpen.CAE.BeamSectionOffsetOptionsMethod

class NXOpen.CAE.BeamSectionOffsetOptionsMethod

Bases: object

Represents the offset definition method

Enum Members

Enum Member Enum Member Description
Neutral
The offset coordindate system is defined in neutral way
LanguageSpecific
The offset coordindate system is defined in language-specific way. Only available to Nastran
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.