PostScenarioManager Class¶
-
class
NXOpen.CAE.
PostScenarioManager
¶ Bases:
object
Manages the creation of a
NXOpen.CAE.PostScenarioBuilder
.To obtain an instance of this class use
NXOpen.CAE.PostScenarioManager()
.New in version NX11.0.0.
“PostScenarioDescriptors”, ” Contains a <ja_class>NXOpen.CAE.PostScenarioDescriptorCollection</ja_class>. “
Methods¶
Method | Description |
---|---|
CheckScenarioDataSourceCompatible | Checks if the scenario and the data source set in the NXOpen.CAE.PostScenarioParameters are compatible. |
CheckValidDataSource | Checks if the data source set in NXOpen.CAE.PostScenarioParameters is valid. |
CreatePostScenarioBuilderFromParameters | Creates a transient object NXOpen.CAE.PostScenarioBuilder that is responsible for creating a post scenario object. |
CreatePostScenarioBuilderFromViewport | Creates a builder for the Scenario retrieved from a Visualized Scenario from a certain viewport. |
NewPostScenarioParameters | Creates a transient object NXOpen.CAE.PostScenarioParameters that contains the settings required to create a post scenario. |
PostScenarioDescriptors¶
-
PostScenarioManager.
PostScenarioDescriptors
¶ Contains a
NXOpen.CAE.PostScenarioDescriptorCollection
.Signature
PostScenarioDescriptors()
New in version NX11.0.0.
Returns: Return type: NXOpen.CAE.PostScenarioDescriptorCollection
Method Detail¶
CheckScenarioDataSourceCompatible¶
-
PostScenarioManager.
CheckScenarioDataSourceCompatible
¶ Checks if the scenario and the data source set in the
NXOpen.CAE.PostScenarioParameters
are compatible.Signature
CheckScenarioDataSourceCompatible(scenarioParameters)
Parameters: scenarioParameters ( NXOpen.CAE.PostScenarioParameters
) –Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CheckValidDataSource¶
-
PostScenarioManager.
CheckValidDataSource
¶ Checks if the data source set in
NXOpen.CAE.PostScenarioParameters
is valid.Signature
CheckValidDataSource(scenarioParameters)
Parameters: scenarioParameters ( NXOpen.CAE.PostScenarioParameters
) –Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreatePostScenarioBuilderFromParameters¶
-
PostScenarioManager.
CreatePostScenarioBuilderFromParameters
¶ Creates a transient object
NXOpen.CAE.PostScenarioBuilder
that is responsible for creating a post scenario object.Signature
CreatePostScenarioBuilderFromParameters(scenarioParameters)
Parameters: scenarioParameters ( NXOpen.CAE.PostScenarioParameters
) –Returns: Return type: NXOpen.CAE.PostScenarioBuilder
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreatePostScenarioBuilderFromViewport¶
-
PostScenarioManager.
CreatePostScenarioBuilderFromViewport
¶ Creates a builder for the Scenario retrieved from a Visualized Scenario from a certain viewport.
This method fails if the specified viewport does not represent a Visualized Scenario.
Signature
CreatePostScenarioBuilderFromViewport(viewportIndex)
Parameters: viewportIndex (int) – Returns: Return type: NXOpen.CAE.PostScenarioBuilder
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
NewPostScenarioParameters¶
-
PostScenarioManager.
NewPostScenarioParameters
¶ Creates a transient object
NXOpen.CAE.PostScenarioParameters
that contains the settings required to create a post scenario.The object should be destroyed after the post scenario is created.
Signature
NewPostScenarioParameters()
Returns: Return type: NXOpen.CAE.PostScenarioParameters
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)