PostScenarioParameters Class¶
-
class
NXOpen.CAE.
PostScenarioParameters
¶ Bases:
NXOpen.TransientObject
The class represents the
NXOpen.CAE.PostScenarioParameters
used to instanciate aNXOpen.CAE.PostScenarioBuilder
.To create a new instance of this class, use
NXOpen.CAE.PostScenarioManager.NewPostScenarioParameters()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
DataSource | Returns or sets the data source object to be processed by the post scenario. |
ScenarioDescriptor | Returns or sets the scenario descriptor used by the post scenario. |
ViewPortIndex | Returns or sets the index of a view port on the main graphic window, on which the plot graph will be shown. |
Property Detail¶
DataSource¶
-
PostScenarioParameters.
DataSource
¶ Returns or sets the data source object to be processed by the post scenario.
-------------------------------------
Getter Method
Signature
DataSource()
Returns: Return type: NXOpen.CAE.IPostScenarioDataSource
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
DataSource(dataSource)
Parameters: dataSource ( NXOpen.CAE.IPostScenarioDataSource
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ScenarioDescriptor¶
-
PostScenarioParameters.
ScenarioDescriptor
¶ Returns or sets the scenario descriptor used by the post scenario.
-------------------------------------
Getter Method
Signature
ScenarioDescriptor()
Returns: Return type: NXOpen.CAE.PostScenarioDescriptor
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
ScenarioDescriptor(scenarioDesc)
Parameters: scenarioDesc ( NXOpen.CAE.PostScenarioDescriptor
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ViewPortIndex¶
-
PostScenarioParameters.
ViewPortIndex
¶ Returns or sets the index of a view port on the main graphic window, on which the plot graph will be shown.
-------------------------------------
Getter Method
Signature
ViewPortIndex()
Returns: Return type: int New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
ViewPortIndex(viewPortIndex)
Parameters: viewPortIndex (int) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)