BoundingVolumeCollection Class¶
-
class
NXOpen.CAE.
BoundingVolumeCollection
¶ Bases:
object
Represents a collection of bounding volumes.
To obtain an instance of this class, refer to
NXOpen.CAE.CaePart
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateBuilder | Creates the builder object of bounding volume. |
FindObject | Finds an bounding volume with a specified name. |
Method Detail¶
CreateBuilder¶
-
BoundingVolumeCollection.
CreateBuilder
¶ Creates the builder object of bounding volume.
Signature
CreateBuilder(boundingVolume)
Parameters: boundingVolume ( NXOpen.CAE.BoundingVolume
) –Returns: Return type: NXOpen.CAE.BoundingVolumeBuilder
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
BoundingVolumeCollection.
FindObject
¶ Finds an bounding volume with a specified name.
Signature
FindObject(name)
Parameters: name (str) – sid of bounding volume Returns: The bounding volume Return type: NXOpen.CAE.BoundingVolume
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)