CAEConnectionCollection Class

class NXOpen.CAE.CAEConnectionCollection

Bases: object

Provides method for creating builder for connection operation commands in a fem/afem part

To obtain an instance of this class, refer to NXOpen.CAE.BaseFEModel

New in version NX6.0.0.

Methods

Method Description
CreateConnectionBuilder Creates a builder for Connection Command @return
CreateWeldConnectionBuilder Creates a builder for WeldConnection Command @return
FindObject Finds the NXOpen.CAE.CAEConnection with the given identifier as recorded in a journal.

Method Detail

CreateConnectionBuilder

CAEConnectionCollection.CreateConnectionBuilder

Creates a builder for Connection Command

Signature CreateConnectionBuilder(connection)

Parameters:connection (NXOpen.CAE.CAEConnection) – NXOpen.CAE.CAEConnection to be edited, if None then create a new one
Returns:
Return type:NXOpen.CAE.CAEConnectionBuilder

New in version NX6.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”)

CreateWeldConnectionBuilder

CAEConnectionCollection.CreateWeldConnectionBuilder

Creates a builder for WeldConnection Command

Signature CreateWeldConnectionBuilder(weldconnection)

Parameters:weldconnection (NXOpen.CAE.CAEWeldConnection) – WeldConnection Recipe to be edited, if None then create a new one
Returns:
Return type:NXOpen.CAE.CAEWeldConnectionBuilder

New in version NX6.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”)

FindObject

CAEConnectionCollection.FindObject

Finds the NXOpen.CAE.CAEConnection with the given identifier as recorded in a journal.

An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.

An exception will be thrown if no object can be found with the given journal identifier.

Signature FindObject(journalIdentifier)

Parameters:journalIdentifier (str) – Connection name
Returns:connection with this identifier
Return type:NXOpen.CAE.CAEConnection

New in version NX6.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”)