CAEConnectionBuilder Class¶
-
class
NXOpen.CAE.
CAEConnectionBuilder
¶ Bases:
NXOpen.Builder
Builder for creating Connection Recipes
To create a new instance of this class, use
NXOpen.CAE.CAEConnectionCollection.CreateConnectionBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
EdgeToEdgeConnectionMethodType | Returns or sets the method type for edge-to-edge connection |
EdgeTolerance | Returns or sets the option to tune edge tolerance. |
ElementEdge | Returns the selected element edge(s) |
ElementFace | Returns the selected element face(s) |
ElementType | Returns the element type to be created |
ElementTypeRbe3 | Returns the element type to be created |
Label | Returns or sets the labeling of elements |
MethodType | Returns or sets the method type for point-point or node-node connections |
MidNode | Returns or sets the mid node option |
SourceGroup | Returns or sets the source group referenced by this connection |
SourceGroupReferenceState | Returns the state defining whether the source of this connection is defined with a group |
SourceNodes | Returns the source Node(s) |
SourceSelection | Returns the selected source object(s) |
Tag | Returns the Tag for this object. |
TargetGroup | Returns or sets the target group referenced by this connection |
TargetGroupReferenceState | Returns the state defining whether the target of this connection is defined with a group |
TargetNodes | Returns the target Node(s) |
TargetSelection | Returns the selected target object(s) |
Type | Returns or sets the connection type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
MeshDensity | The mesh density setting |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CAEConnectionBuilderConnectionTypeEnum Enumeration | the type of connection to be created |
CAEConnectionBuilderEdgeToEdgeConnectionMethodTypeEnum Enumeration | the method of edge to edge connection to be created |
CAEConnectionBuilderMethodTypeEnum Enumeration | the method of connection to be created |
Property Detail¶
EdgeToEdgeConnectionMethodType¶
-
CAEConnectionBuilder.
EdgeToEdgeConnectionMethodType
¶ Returns or sets the method type for edge-to-edge connection
-------------------------------------
Getter Method
Signature
EdgeToEdgeConnectionMethodType()
Returns: Return type: NXOpen.CAE.CAEConnectionBuilderEdgeToEdgeConnectionMethodTypeEnum
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EdgeToEdgeConnectionMethodType(edgeToEdgeConnectionMethodType)
Parameters: edgeToEdgeConnectionMethodType ( NXOpen.CAE.CAEConnectionBuilderEdgeToEdgeConnectionMethodTypeEnum
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EdgeTolerance¶
-
CAEConnectionBuilder.
EdgeTolerance
¶ Returns or sets the option to tune edge tolerance.
-------------------------------------
Getter Method
Signature
EdgeTolerance()
Returns: Return type: float New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
EdgeTolerance(edgeTolerance)
Parameters: edgeTolerance (float) – New in version NX8.0.1.
License requirements: None.
ElementEdge¶
-
CAEConnectionBuilder.
ElementEdge
¶ Returns the selected element edge(s)
-------------------------------------
Getter Method
Signature
ElementEdge()
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX6.0.0.
License requirements: None.
ElementFace¶
-
CAEConnectionBuilder.
ElementFace
¶ Returns the selected element face(s)
-------------------------------------
Getter Method
Signature
ElementFace()
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX6.0.0.
License requirements: None.
ElementType¶
-
CAEConnectionBuilder.
ElementType
¶ Returns the element type to be created
-------------------------------------
Getter Method
Signature
ElementType()
Returns: Return type: NXOpen.CAE.ElementTypeBuilder
New in version NX6.0.0.
License requirements: None.
ElementTypeRbe3¶
-
CAEConnectionBuilder.
ElementTypeRbe3
¶ Returns the element type to be created
-------------------------------------
Getter Method
Signature
ElementTypeRbe3()
Returns: Return type: NXOpen.CAE.ElementTypeBuilder
New in version NX6.0.1.
License requirements: None.
Label¶
-
CAEConnectionBuilder.
Label
¶ Returns or sets the labeling of elements
-------------------------------------
Getter Method
Signature
Label()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label(label)
Parameters: label (int) – New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MethodType¶
-
CAEConnectionBuilder.
MethodType
¶ Returns or sets the method type for point-point or node-node connections
-------------------------------------
Getter Method
Signature
MethodType()
Returns: Return type: NXOpen.CAE.CAEConnectionBuilderMethodTypeEnum
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MethodType(methodType)
Parameters: methodType ( NXOpen.CAE.CAEConnectionBuilderMethodTypeEnum
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MidNode¶
-
CAEConnectionBuilder.
MidNode
¶ Returns or sets the mid node option
-------------------------------------
Getter Method
Signature
MidNode()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MidNode(midNode)
Parameters: midNode (bool) – New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SourceGroup¶
-
CAEConnectionBuilder.
SourceGroup
¶ Returns or sets the source group referenced by this connection
-------------------------------------
Getter Method
Signature
SourceGroup()
Returns: Return type: NXOpen.CAE.CaeGroup
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
SourceGroup(groupToRef)
Parameters: groupToRef ( NXOpen.CAE.CaeGroup
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SourceGroupReferenceState¶
-
CAEConnectionBuilder.
SourceGroupReferenceState
¶ Returns the state defining whether the source of this connection is defined with a group
-------------------------------------
Getter Method
Signature
SourceGroupReferenceState()
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SourceNodes¶
-
CAEConnectionBuilder.
SourceNodes
¶ Returns the source Node(s)
-------------------------------------
Getter Method
Signature
SourceNodes()
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX6.0.0.
License requirements: None.
SourceSelection¶
-
CAEConnectionBuilder.
SourceSelection
¶ Returns the selected source object(s)
-------------------------------------
Getter Method
Signature
SourceSelection()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX6.0.0.
License requirements: None.
TargetGroup¶
-
CAEConnectionBuilder.
TargetGroup
¶ Returns or sets the target group referenced by this connection
-------------------------------------
Getter Method
Signature
TargetGroup()
Returns: Return type: NXOpen.CAE.CaeGroup
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
TargetGroup(groupToRef)
Parameters: groupToRef ( NXOpen.CAE.CaeGroup
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
TargetGroupReferenceState¶
-
CAEConnectionBuilder.
TargetGroupReferenceState
¶ Returns the state defining whether the target of this connection is defined with a group
-------------------------------------
Getter Method
Signature
TargetGroupReferenceState()
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
TargetNodes¶
-
CAEConnectionBuilder.
TargetNodes
¶ Returns the target Node(s)
-------------------------------------
Getter Method
Signature
TargetNodes()
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX6.0.0.
License requirements: None.
TargetSelection¶
-
CAEConnectionBuilder.
TargetSelection
¶ Returns the selected target object(s)
-------------------------------------
Getter Method
Signature
TargetSelection()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX6.0.0.
License requirements: None.
Type¶
-
CAEConnectionBuilder.
Type
¶ Returns or sets the connection type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.CAE.CAEConnectionBuilderConnectionTypeEnum
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(connectionType)
Parameters: connectionType ( NXOpen.CAE.CAEConnectionBuilderConnectionTypeEnum
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
MeshDensity¶
-
CAEConnectionBuilder.
MeshDensity
¶ The mesh density setting
Signature
MeshDensity()
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
CAEConnectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.