FemCreationOptionsUseBodiesOption Enumeration¶
NXOpen.CAE.FemCreationOptions.UseBodiesOption is an alias for NXOpen.CAE.FemCreationOptionsUseBodiesOption
-
class
NXOpen.CAE.
FemCreationOptionsUseBodiesOption
¶ Bases:
object
Used to specify the option of specifying bodies to use from the CAD Part while creating
CAE.FemPart
.Enum Members
Enum Member Enum Member Description SelectedBodies Use selected bodies from the cad partVisibleBodies Use all visible bodies from the cad partAllBodies Use all bodies from the cad part-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-