DurabilityStressAxesBuilderNodeElementOptionEnum Enumeration

NXOpen.CAE.DurabilityStressAxesBuilder.NodeElementOptionEnum is an alias for NXOpen.CAE.DurabilityStressAxesBuilderNodeElementOptionEnum

class NXOpen.CAE.DurabilityStressAxesBuilderNodeElementOptionEnum

Bases: object

the Node Element Option Enum.

Enum Members

Enum Member Enum Member Description
Solids
Solids
Shells
Shells
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.