DurabilityEventStrengthSettingsBuilderStressTypeEnum Enumeration

NXOpen.CAE.DurabilityEventStrengthSettingsBuilder.StressTypeEnum is an alias for NXOpen.CAE.DurabilityEventStrengthSettingsBuilderStressTypeEnum

class NXOpen.CAE.DurabilityEventStrengthSettingsBuilderStressTypeEnum

Bases: object

the stress type enum.

Enum Members

Enum Member Enum Member Description
VonMises
Von Mises
Tresca
Tresca
MaximumPrincipal
Maximum Principal
MinimumPrincipal
Minimum Principal
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.