GroupElemMethod Class

class NXOpen.CAE.GroupElemMethod

Bases: NXOpen.SelectionMethod

Represents the output from the Group Element smart selector method

To obtain an instance of this class use CAE::SmartSelectionManager

New in version NX6.0.0.

Methods

Method Description
Dispose Frees the object from memory.
GetElements Returns the resultant elements @return Resultant elements
GetSelectedObjects Returns the objects selected by this NXOpen.SelectionMethod.

Method Detail

Dispose

GroupElemMethod.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX6.0.0.

License requirements: None.

GetElements

GroupElemMethod.GetElements

Returns the resultant elements

Signature GetElements()

Returns:Resultant elements
Return type:list of NXOpen.CAE.FEElement

New in version NX6.0.4.

License requirements: None.