MergeFaceBuilder Class¶
-
class
NXOpen.CAE.
MergeFaceBuilder
¶ Bases:
NXOpen.Builder
Builder for creating Merge Face
To create a new instance of this class, use
NXOpen.CAE.AbstractionManager.CreateMergeFaceBuilder()
Default values.
Property Value AutoRemoveToggle 1 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AutoRemoveToggle | Returns or sets the auto remove the soft vertices option |
EdgeAngle | Returns the edge angle criterion is used to merge faces at an angle |
SelectEdgeFaceBodyBlock | Returns the geom selection for intersection curve |
Tag | Returns the Tag for this object. |
VertexAngle | Returns the vertex angle criterion is used to remove soft vertices |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AutoRemoveToggle¶
-
MergeFaceBuilder.
AutoRemoveToggle
¶ Returns or sets the auto remove the soft vertices option
-------------------------------------
Getter Method
Signature
AutoRemoveToggle()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutoRemoveToggle(autoremovetoggle)
Parameters: autoremovetoggle (bool) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EdgeAngle¶
-
MergeFaceBuilder.
EdgeAngle
¶ Returns the edge angle criterion is used to merge faces at an angle
-------------------------------------
Getter Method
Signature
EdgeAngle()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
SelectEdgeFaceBodyBlock¶
-
MergeFaceBuilder.
SelectEdgeFaceBodyBlock
¶ Returns the geom selection for intersection curve
-------------------------------------
Getter Method
Signature
SelectEdgeFaceBodyBlock()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX11.0.0.
License requirements: None.
VertexAngle¶
-
MergeFaceBuilder.
VertexAngle
¶ Returns the vertex angle criterion is used to remove soft vertices
-------------------------------------
Getter Method
Signature
VertexAngle()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
MergeFaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.