AbstractionManager Class¶
-
class
NXOpen.CAE.
AbstractionManager
¶ Bases:
object
Provides method for creating builder for abstraction commands in a fem part
To obtain an instance of this class, refer to
NXOpen.CAE.FEModel
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
CreateCircularImprintBuilder | Creates a builder for abstraction Command @return |
CreateDeletePolygonFaceBuilder | Creates a NXOpen.CAE.DeletePolygonFaceBuilder @return |
CreateEdgeFaceImprintBuilder | Creates a NXOpen.CAE.EdgeFaceImprintBuilder . |
CreateFaceFaceImprintBuilder | Creates a NXOpen.CAE.FaceFaceImprintBuilder . |
CreateFaceFromBoundaryBuilder | Creates a NXOpen.CAE.FaceFromBoundaryBuilder @return |
CreateImprintBuilder | Creates a NXOpen.CAE.ImprintBuilder This class is not yet SUPPORTED for use. |
CreateMergeFaceBuilder | Creates a NXOpen.CAE.MergeFaceBuilder @return |
CreatePolygonFaceOnMeshBuilder | Creates a builder for Polygon Face On Mesh Command @return |
CreateSuppressHoleBuilder | Creates a builder for Suppress Hole Command @return |
Method Detail¶
CreateCircularImprintBuilder¶
-
AbstractionManager.
CreateCircularImprintBuilder
¶ Creates a builder for abstraction Command
Signature
CreateCircularImprintBuilder()
Returns: Return type: NXOpen.CAE.CircularImprintBuilder
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateDeletePolygonFaceBuilder¶
-
AbstractionManager.
CreateDeletePolygonFaceBuilder
¶ Creates a
NXOpen.CAE.DeletePolygonFaceBuilder
Signature
CreateDeletePolygonFaceBuilder()
Returns: Return type: NXOpen.CAE.DeletePolygonFaceBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateEdgeFaceImprintBuilder¶
-
AbstractionManager.
CreateEdgeFaceImprintBuilder
¶ Creates a
NXOpen.CAE.EdgeFaceImprintBuilder
.This class is not yet SUPPORTED for use.
Signature
CreateEdgeFaceImprintBuilder()
Returns: Return type: NXOpen.CAE.EdgeFaceImprintBuilder
New in version NX11.0.0.
Deprecated since version NX11.0.0: Use
CAE.ImprintBuilder
.License requirements: nx_masterfem (“Finite Element Modeling”)
CreateFaceFaceImprintBuilder¶
-
AbstractionManager.
CreateFaceFaceImprintBuilder
¶ Creates a
NXOpen.CAE.FaceFaceImprintBuilder
.This class is not yet SUPPORTED for use.
Signature
CreateFaceFaceImprintBuilder()
Returns: Return type: NXOpen.CAE.FaceFaceImprintBuilder
New in version NX11.0.0.
Deprecated since version NX11.0.0: Use
CAE.ImprintBuilder
.License requirements: nx_masterfem (“Finite Element Modeling”)
CreateFaceFromBoundaryBuilder¶
-
AbstractionManager.
CreateFaceFromBoundaryBuilder
¶ Creates a
NXOpen.CAE.FaceFromBoundaryBuilder
Signature
CreateFaceFromBoundaryBuilder()
Returns: Return type: NXOpen.CAE.FaceFromBoundaryBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateImprintBuilder¶
-
AbstractionManager.
CreateImprintBuilder
¶ Creates a
NXOpen.CAE.ImprintBuilder
This class is not yet SUPPORTED for use.Signature
CreateImprintBuilder()
Returns: Return type: NXOpen.CAE.ImprintBuilder
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateMergeFaceBuilder¶
-
AbstractionManager.
CreateMergeFaceBuilder
¶ Creates a
NXOpen.CAE.MergeFaceBuilder
Signature
CreateMergeFaceBuilder()
Returns: Return type: NXOpen.CAE.MergeFaceBuilder
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreatePolygonFaceOnMeshBuilder¶
-
AbstractionManager.
CreatePolygonFaceOnMeshBuilder
¶ Creates a builder for Polygon Face On Mesh Command
Signature
CreatePolygonFaceOnMeshBuilder()
Returns: Return type: NXOpen.CAE.PolygonFaceOnMeshBuilder
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateSuppressHoleBuilder¶
-
AbstractionManager.
CreateSuppressHoleBuilder
¶ Creates a builder for Suppress Hole Command
Signature
CreateSuppressHoleBuilder()
Returns: Return type: NXOpen.CAE.SuppressHoleBuilder
New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)