PolygonFaceOnMeshBuilder Class¶
-
class
NXOpen.CAE.
PolygonFaceOnMeshBuilder
¶ Bases:
NXOpen.Builder
Builder for creating Polygon Face On Mesh
To create a new instance of this class, use
NXOpen.CAE.AbstractionManager.CreatePolygonFaceOnMeshBuilder()
New in version NX7.5.2.
Properties¶
Property | Description |
---|---|
BoundaryMerging | Returns the angle |
ElementSelection | Returns the selected element(s) |
FaceSmoothing | Returns the angle |
SelectBody | Returns the selected body |
SelectBodyOption | Returns or sets the select body option for different ways of body select method |
Tag | Returns the Tag for this object. |
Type | Returns or sets the selection method for different ways of selection |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PolygonFaceOnMeshBuilderPolygonFaceOnMeshType Enumeration | Represents the polygon face on mesh type to be used |
PolygonFaceOnMeshBuilderSelectBodyMethod Enumeration | Represents the select body option to be used |
Property Detail¶
BoundaryMerging¶
-
PolygonFaceOnMeshBuilder.
BoundaryMerging
¶ Returns the angle
-------------------------------------
Getter Method
Signature
BoundaryMerging()
Returns: Return type: NXOpen.Expression
New in version NX7.5.2.
License requirements: None.
ElementSelection¶
-
PolygonFaceOnMeshBuilder.
ElementSelection
¶ Returns the selected element(s)
-------------------------------------
Getter Method
Signature
ElementSelection()
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX7.5.2.
License requirements: None.
FaceSmoothing¶
-
PolygonFaceOnMeshBuilder.
FaceSmoothing
¶ Returns the angle
-------------------------------------
Getter Method
Signature
FaceSmoothing()
Returns: Return type: NXOpen.Expression
New in version NX7.5.2.
License requirements: None.
SelectBody¶
-
PolygonFaceOnMeshBuilder.
SelectBody
¶ Returns the selected body
-------------------------------------
Getter Method
Signature
SelectBody()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
SelectBodyOption¶
-
PolygonFaceOnMeshBuilder.
SelectBodyOption
¶ Returns or sets the select body option for different ways of body select method
-------------------------------------
Getter Method
Signature
SelectBodyOption()
Returns: Return type: NXOpen.CAE.PolygonFaceOnMeshBuilderSelectBodyMethod
New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectBodyOption(selectBodyMethod)
Parameters: selectBodyMethod ( NXOpen.CAE.PolygonFaceOnMeshBuilderSelectBodyMethod
) –New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
Type¶
-
PolygonFaceOnMeshBuilder.
Type
¶ Returns or sets the selection method for different ways of selection
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.CAE.PolygonFaceOnMeshBuilderPolygonFaceOnMeshType
New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(selectionType)
Parameters: selectionType ( NXOpen.CAE.PolygonFaceOnMeshBuilderPolygonFaceOnMeshType
) –New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
PolygonFaceOnMeshBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.