PolygonFaceOnMeshBuilderSelectBodyMethod Enumeration

NXOpen.CAE.PolygonFaceOnMeshBuilder.SelectBodyMethod is an alias for NXOpen.CAE.PolygonFaceOnMeshBuilderSelectBodyMethod

class NXOpen.CAE.PolygonFaceOnMeshBuilderSelectBodyMethod

Bases: object

Represents the select body option to be used

Enum Members

Enum Member Enum Member Description
CreateNew
Create new body
AddToExisting
Add to existing body
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.