PostScenarioVariable Class

class NXOpen.CAE.PostScenarioVariable

Bases: NXOpen.TaggedObject

A selection variable to which values can be bound in order to define a user selection for a post scenario. See NXOpen.CAE.PostScenarioSelectionParameters

Not support KF.

New in version NX11.0.0.

Properties

Property Description
DisplayName Returns the localized name of this Variable.
Name Returns the name of this Variable.
Tag Returns the Tag for this object.

Methods

Method Description
AssignBooleanValues Assign boolean values to this Selection Variable.
AssignComplexValues Assign complex values to this Selection Variable.
AssignDoubleValues Assign double values to this Selection Variable.
AssignIntegerValues Assign integer values to this Selection Variable.
AssignStringValues Assign string values to this Selection Variable.
AssignUnicodeStringValues Assign unicode string values to this Selection Variable.
AssignValues Assign variant values to this Selection Variable.
GetValues Read the available values of this variable.

Property Detail

DisplayName

PostScenarioVariable.DisplayName

Returns the localized name of this Variable.

-------------------------------------

Getter Method

Signature DisplayName()

Returns:
Return type:str

New in version NX11.0.0.

License requirements: None.

Name

PostScenarioVariable.Name

Returns the name of this Variable.

-------------------------------------

Getter Method

Signature Name()

Returns:
Return type:str

New in version NX11.0.0.

License requirements: None.

Method Detail

AssignBooleanValues

PostScenarioVariable.AssignBooleanValues

Assign boolean values to this Selection Variable.

The assigned values must be a subset of the values returned by GetValues, otherwise an exception is raised.

Signature AssignBooleanValues(values)

Parameters:values (list of bool) –

New in version NX11.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

AssignComplexValues

PostScenarioVariable.AssignComplexValues

Assign complex values to this Selection Variable.

The assigned values must be a subset of the values returned by GetValues, otherwise an exception is raised.

Signature AssignComplexValues(values)

Parameters:values (list of NXOpen.CAE.Complex) –

New in version NX11.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

AssignDoubleValues

PostScenarioVariable.AssignDoubleValues

Assign double values to this Selection Variable.

The assigned values must be a subset of the values returned by GetValues, otherwise an exception is raised.

Signature AssignDoubleValues(values)

Parameters:values (list of float) –

New in version NX11.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

AssignIntegerValues

PostScenarioVariable.AssignIntegerValues

Assign integer values to this Selection Variable.

The assigned values must be a subset of the values returned by GetValues, otherwise an exception is raised.

Signature AssignIntegerValues(values)

Parameters:values (list of int) –

New in version NX11.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

AssignStringValues

PostScenarioVariable.AssignStringValues

Assign string values to this Selection Variable.

The assigned values must be a subset of the values returned by GetValues, otherwise an exception is raised.

Signature AssignStringValues(values)

Parameters:values (list of str) –

New in version NX11.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

AssignUnicodeStringValues

PostScenarioVariable.AssignUnicodeStringValues

Assign unicode string values to this Selection Variable.

The assigned values must be a subset of the values returned by GetValues, otherwise an exception is raised.

Signature AssignUnicodeStringValues(values)

Parameters:values (list of str) –

New in version NX11.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

AssignValues

PostScenarioVariable.AssignValues

Assign variant values to this Selection Variable.

The assigned values must be a subset of the values returned by GetValues, otherwise an exception is raised.

Signature AssignValues(values)

Parameters:values (list of NXOpen.CAE.PostScenarioVariant) –

New in version NX11.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

GetValues

PostScenarioVariable.GetValues

Read the available values of this variable.

The returned values have to be disposed explicitely. This returns all the possible values which can be assigned to this PostScenarioVariable.

Signature GetValues()

Returns:
Return type:list of NXOpen.CAE.PostScenarioVariant

New in version NX11.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)