PostScenarioSelectionParameters Class¶
-
class
NXOpen.CAE.
PostScenarioSelectionParameters
¶ Bases:
NXOpen.TaggedObject
The class handles the User Selection for a Scenario.
A User Selection identifies which data need to be retrieved from the data source on top of which a scenario was created. A User Selection is dependent on the previously selected
NXOpen.CAE.PostScenarioInputDefinition
, Data SourceNXOpen.CAE.PostScenarioDataDefinition
, andNXOpen.CAE.PostScenarioVisualizationDefinition
. SeeNXOpen.CAE.PostScenarioBuilder
. An instance can be created from a CAE.PostScenarioBuilder.A valid user selection binds at least one value to each
NXOpen.CAE.PostScenarioVariable
. The exact constraints on the number of selected values varies which each scenario.In order to bind values to variables, one must access each Variable from the
NXOpen.CAE.PostScenarioVariableCollection
, and bind values from those which are listed by the Variable’sNXOpen.CAE.PostScenarioVariable.GetValues()
method.:py:class:`NXOpen.CAE.PostScenarioConfigurationVariable`s are Scenario specific and enable or configure scenario specific behaviour.
Not support KF.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
Variables |
|
ConfigurationVariables |
|
Methods¶
Method | Description |
---|---|
NewVariant | Create a new NXOpen.CAE.PostScenarioVariant that wraps a scalar value. |
Variables¶
-
PostScenarioSelectionParameters.
Variables
¶ Contains selection :py:class:`NXOpen.CAE.PostScenarioVariable`s that define this selection.
Signature
Variables()
New in version NX11.0.0.
Returns: Return type: NXOpen.CAE.PostScenarioVariableCollection
ConfigurationVariables¶
-
PostScenarioSelectionParameters.
ConfigurationVariables
¶ Contains :py:class:`NXOpen.CAE.PostScenarioConfigurationVariable`s for this selection.
Signature
ConfigurationVariables()
New in version NX11.0.0.
Returns: Return type: NXOpen.CAE.PostScenarioConfigurationVariableCollection
Method Detail¶
NewVariant¶
-
PostScenarioSelectionParameters.
NewVariant
¶ Create a new
NXOpen.CAE.PostScenarioVariant
that wraps a scalar value.These objects need to be Dispose’d of once it is no longer needed.
Signature
NewVariant()
Returns: Return type: NXOpen.CAE.PostScenarioVariant
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)