InterpolationEADBuilder Class¶
-
class
NXOpen.CAE.
InterpolationEADBuilder
¶ Bases:
NXOpen.Builder
This class provides Interpolation Associated Data Support
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateInterpolationEadBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Elements | Returns the select element operator selects elements |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDof1Weights | The get dof1_weights operator gets dof 1 weight values @return |
GetDof2Weights | The get dof2_weights operator gets dof 2 weight values @return |
GetDof3Weights | The get dof3_weights operator gets dof 3 weight values @return |
GetDof4Weights | The get dof4_weights operator gets dof 4 weight values @return |
GetDof5Weights | The get dof5_weights operator gets dof 5 weight values @return |
GetDof6Weights | The get dof6_weights operator gets dof 6 weight values @return |
GetObject | Returns the object currently being edited by this builder. |
GetUmData | The get_um_data operator gets the array of 12 um_data values @return |
SetDof1Weights | The set_dof1_weights operator selects elements |
SetDof2Weights | The set_dof2_weights operator selects elements |
SetDof3Weights | The set_dof3_weights operator selects elements |
SetDof4Weights | The set_dof4_weights operator selects elements |
SetDof5Weights | The set_dof5_weights operator selects elements |
SetDof6Weights | The set_dof6_weights operator selects elements |
SetUmData | The set_um_data operator sets the array of 12 um_data values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Elements¶
-
InterpolationEADBuilder.
Elements
¶ Returns the select element operator selects elements
-------------------------------------
Getter Method
Signature
Elements()
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
GetDof1Weights¶
-
InterpolationEADBuilder.
GetDof1Weights
¶ The get dof1_weights operator gets dof 1 weight values
Signature
GetDof1Weights()
Returns: Return type: list of float New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetDof2Weights¶
-
InterpolationEADBuilder.
GetDof2Weights
¶ The get dof2_weights operator gets dof 2 weight values
Signature
GetDof2Weights()
Returns: Return type: list of float New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetDof3Weights¶
-
InterpolationEADBuilder.
GetDof3Weights
¶ The get dof3_weights operator gets dof 3 weight values
Signature
GetDof3Weights()
Returns: Return type: list of float New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetDof4Weights¶
-
InterpolationEADBuilder.
GetDof4Weights
¶ The get dof4_weights operator gets dof 4 weight values
Signature
GetDof4Weights()
Returns: Return type: list of float New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetDof5Weights¶
-
InterpolationEADBuilder.
GetDof5Weights
¶ The get dof5_weights operator gets dof 5 weight values
Signature
GetDof5Weights()
Returns: Return type: list of float New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetDof6Weights¶
-
InterpolationEADBuilder.
GetDof6Weights
¶ The get dof6_weights operator gets dof 6 weight values
Signature
GetDof6Weights()
Returns: Return type: list of float New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetUmData¶
-
InterpolationEADBuilder.
GetUmData
¶ The get_um_data operator gets the array of 12 um_data values
Signature
GetUmData()
Returns: Return type: list of int New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetDof1Weights¶
-
InterpolationEADBuilder.
SetDof1Weights
¶ The set_dof1_weights operator selects elements
Signature
SetDof1Weights(dofWeights)
Parameters: dofWeights (list of float) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetDof2Weights¶
-
InterpolationEADBuilder.
SetDof2Weights
¶ The set_dof2_weights operator selects elements
Signature
SetDof2Weights(dofWeights)
Parameters: dofWeights (list of float) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetDof3Weights¶
-
InterpolationEADBuilder.
SetDof3Weights
¶ The set_dof3_weights operator selects elements
Signature
SetDof3Weights(dofWeights)
Parameters: dofWeights (list of float) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetDof4Weights¶
-
InterpolationEADBuilder.
SetDof4Weights
¶ The set_dof4_weights operator selects elements
Signature
SetDof4Weights(dofWeights)
Parameters: dofWeights (list of float) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetDof5Weights¶
-
InterpolationEADBuilder.
SetDof5Weights
¶ The set_dof5_weights operator selects elements
Signature
SetDof5Weights(dofWeights)
Parameters: dofWeights (list of float) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetDof6Weights¶
-
InterpolationEADBuilder.
SetDof6Weights
¶ The set_dof6_weights operator selects elements
Signature
SetDof6Weights(dofWeights)
Parameters: dofWeights (list of float) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetUmData¶
-
InterpolationEADBuilder.
SetUmData
¶ The set_um_data operator sets the array of 12 um_data values
Signature
SetUmData(umData)
Parameters: umData (list of int) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
InterpolationEADBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.