NodeElementManager Class¶
-
class
NXOpen.CAE.
NodeElementManager
¶ Bases:
object
Provides method for creating builder for node element operation commands in a fem part
To obtain an instance of this class, refer to
NXOpen.CAE.BaseFEModel
New in version NX5.0.0.
“ElemInfoUtils”, ” Returns the element information utility “
Methods¶
Method | Description |
---|---|
CreateAttachElementsBuilder | Creates a builder for attach elements command @return |
CreateAutomaticMorphBuilder | Creates a builder for Automatic Morphing command @return |
CreateBeamEadBuilder | Creates a builder for the Beam EAD block. |
CreateBushingEadBuilder | Creates a builder for the Bushing EAD block. |
CreateCombineTrisBuilder | Creates a builder for Combine Tris. |
CreateConvexMeshBuilder | Creates a NXOpen.CAE.ConvexMeshBuilder @return |
CreateDeleteElementBuilder | Creates a builder for element delete command @return |
CreateDestinationCollectorBuilder | Creates a builder for the Destination Collector Specification block. |
CreateElementConnectivityBuilder | Creates a builder for element connectivity command @return |
CreateElementCreateBuilder | Creates a builder for element create command @return |
CreateElementDetachBuilder | Creates a builder for element detach command @return |
CreateElementExtractBuilder | Creates a builder for Element Extract. |
CreateElementExtrudeBuilder | Creates a builder for element extrude command @return |
CreateElementModifyLabelBuilder | Creates a builder for element modify label command @return |
CreateElementModifyOrderBuilder | Creates a builder for element modify order command @return |
CreateElementModifyTypeBuilder | Creates a builder for element modify type command @return |
CreateElementProjectBuilder | Creates a builder for element project command @return |
CreateElementReflectBuilder | Creates a builder for element reflect command @return |
CreateElementRevolveBuilder | Creates a builder for element revolve command @return |
CreateElementSplitBuilder | Creates a builder for element split command @return |
CreateElementTranslateBuilder | Creates a builder for element translate command @return |
CreateElementTypeBuilder | Creates a builder for the Element Type Specification block. |
CreateGapEadBuilder | Creates a builder for the Gap EAD block. |
CreateInterpolationEadBuilder | Creates a builder for the Interpolation EAD block and initializes it with the input element if defined. |
CreateLumpedMassEadBuilder | Creates a builder for the Lumped Mass EAD block. |
CreateManualMorphBuilder | Creates a builder for Manual Morphing command @return |
CreateManualNodeAssociationBuilder | Creates a builder for manual node association command @return |
CreateMeshFromBoundaryBuilder | Creates Mesh From Boundary builder. |
CreateMorphRevolvedMeshBuilder | Creates a NXOpen.CAE.MorphRevolvedMeshBuilder @return |
CreateMultipleElementCreateBuilder | Creates a builder for the creation of multiple elements. |
CreateMultipleNodeCreateBuilder | Creates a builder for the creation of multiple nodes. |
CreateNodeAlignBuilder | Creates a builder for node align command @return |
CreateNodeAssociationBuilder | Creates a builder for node association command @return |
CreateNodeCreateBuilder | Creates a builder for node create command @return |
CreateNodeDeleteBuilder | Creates a builder for node delete command @return |
CreateNodeDissociationBuilder | Creates a builder for node dissociation command @return |
CreateNodeModifyLabelBuilder | Creates a builder for node modify label command @return |
CreateNodeModifyLocationBuilder | Creates a builder for node modify location command @return |
CreateNodeProjectBuilder | Creates a builder for node project command @return |
CreateNodeReflectBuilder | Creates a builder for Node reflect command @return |
CreateNodeRotateBuilder | Creates a builder for node rotate command @return |
CreateNodeTranslateBuilder | Creates a builder for node translate command @return |
CreateNodesBetweenNodesBuilder | Creates a builder for node between nodes command @return |
CreateNodesOnCurveBuilder | Creates a builder for nodes on curve command @return |
CreateNodesRepositionBuilder | Creates a builder for repositioning nodes, Use this command when you need to modify many nodes at one time. |
CreateOneDimensionalElementSplitBuilder | Creates a builder for one dimensional element split command @return |
CreateRemoveRibsBuilder | Creates a builder for remove ribs command @return |
CreateShellEadBuilder | Creates a builder for the Shell EAD block. |
CreateSpiderElementBuilder | Creates a builder for spider element command @return |
CreateSpringEadBuilder | Creates a builder for the Spring EAD block. |
CreateSurfaceCoatBuilder | Creates a builder for the Surface Coat. |
CreateSweepBetweenMeshBuilder | Creates a builder for Manual Hex Mesh. |
CreateThickenMeshBuilder | Creates a NXOpen.CAE.ThickenMeshBuilder @return |
ElemInfoUtils¶
-
NodeElementManager.
ElemInfoUtils
¶ Returns the element information utility
Signature
ElemInfoUtils()
New in version NX11.0.0.
Returns: Return type: NXOpen.CAE.ElementInfoUtils
Method Detail¶
CreateAttachElementsBuilder¶
-
NodeElementManager.
CreateAttachElementsBuilder
¶ Creates a builder for attach elements command
Signature
CreateAttachElementsBuilder()
Returns: Return type: NXOpen.CAE.AttachElementsBuilder
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateAutomaticMorphBuilder¶
-
NodeElementManager.
CreateAutomaticMorphBuilder
¶ Creates a builder for Automatic Morphing command
Signature
CreateAutomaticMorphBuilder()
Returns: Return type: NXOpen.CAE.AutomaticMorphBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateBeamEadBuilder¶
-
NodeElementManager.
CreateBeamEadBuilder
¶ Creates a builder for the Beam EAD block.
Signature
CreateBeamEadBuilder()
Returns: Return type: NXOpen.CAE.BeamEADBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateBushingEadBuilder¶
-
NodeElementManager.
CreateBushingEadBuilder
¶ Creates a builder for the Bushing EAD block.
Signature
CreateBushingEadBuilder()
Returns: Return type: NXOpen.CAE.BushingEADBuilder
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateCombineTrisBuilder¶
-
NodeElementManager.
CreateCombineTrisBuilder
¶ Creates a builder for Combine Tris.
Signature
CreateCombineTrisBuilder()
Returns: Return type: NXOpen.CAE.CombineTrisBuilder
New in version NX7.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateConvexMeshBuilder¶
-
NodeElementManager.
CreateConvexMeshBuilder
¶ Creates a
NXOpen.CAE.ConvexMeshBuilder
Signature
CreateConvexMeshBuilder()
Returns: Return type: NXOpen.CAE.ConvexMeshBuilder
New in version NX11.0.0.
License requirements: nx_acoustic_modeling (” NX Acoustic Modeling”)
CreateDeleteElementBuilder¶
-
NodeElementManager.
CreateDeleteElementBuilder
¶ Creates a builder for element delete command
Signature
CreateDeleteElementBuilder()
Returns: Return type: NXOpen.CAE.ElementDeleteBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateDestinationCollectorBuilder¶
-
NodeElementManager.
CreateDestinationCollectorBuilder
¶ Creates a builder for the Destination Collector Specification block.
Signature
CreateDestinationCollectorBuilder(isInEdit, elementTypeBuilder)
Parameters: - isInEdit (bool) – the parent builder is editng an existing mesh/element collection.
- elementTypeBuilder (
NXOpen.CAE.ElementTypeBuilder
) – the element type specification block
Returns: Return type: New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementConnectivityBuilder¶
-
NodeElementManager.
CreateElementConnectivityBuilder
¶ Creates a builder for element connectivity command
Signature
CreateElementConnectivityBuilder()
Returns: Return type: NXOpen.CAE.ElementConnectivityBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementCreateBuilder¶
-
NodeElementManager.
CreateElementCreateBuilder
¶ Creates a builder for element create command
Signature
CreateElementCreateBuilder()
Returns: Return type: NXOpen.CAE.ElementCreateBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementDetachBuilder¶
-
NodeElementManager.
CreateElementDetachBuilder
¶ Creates a builder for element detach command
Signature
CreateElementDetachBuilder()
Returns: Return type: NXOpen.CAE.ElementDetachBuilder
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementExtractBuilder¶
-
NodeElementManager.
CreateElementExtractBuilder
¶ Creates a builder for Element Extract.
Signature
CreateElementExtractBuilder()
Returns: Return type: NXOpen.CAE.ElementExtractBuilder
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementExtrudeBuilder¶
-
NodeElementManager.
CreateElementExtrudeBuilder
¶ Creates a builder for element extrude command
Signature
CreateElementExtrudeBuilder()
Returns: Return type: NXOpen.CAE.ElementExtrudeBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementModifyLabelBuilder¶
-
NodeElementManager.
CreateElementModifyLabelBuilder
¶ Creates a builder for element modify label command
Signature
CreateElementModifyLabelBuilder()
Returns: Return type: NXOpen.CAE.ElementModifyLabelBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementModifyOrderBuilder¶
-
NodeElementManager.
CreateElementModifyOrderBuilder
¶ Creates a builder for element modify order command
Signature
CreateElementModifyOrderBuilder()
Returns: Return type: NXOpen.CAE.ElementModifyOrderBuilder
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementModifyTypeBuilder¶
-
NodeElementManager.
CreateElementModifyTypeBuilder
¶ Creates a builder for element modify type command
Signature
CreateElementModifyTypeBuilder()
Returns: Return type: NXOpen.CAE.ElementModifyTypeBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementProjectBuilder¶
-
NodeElementManager.
CreateElementProjectBuilder
¶ Creates a builder for element project command
Signature
CreateElementProjectBuilder()
Returns: Return type: NXOpen.CAE.ElementProjectBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementReflectBuilder¶
-
NodeElementManager.
CreateElementReflectBuilder
¶ Creates a builder for element reflect command
Signature
CreateElementReflectBuilder()
Returns: Return type: NXOpen.CAE.ElementReflectBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementRevolveBuilder¶
-
NodeElementManager.
CreateElementRevolveBuilder
¶ Creates a builder for element revolve command
Signature
CreateElementRevolveBuilder()
Returns: Return type: NXOpen.CAE.ElementRevolveBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementSplitBuilder¶
-
NodeElementManager.
CreateElementSplitBuilder
¶ Creates a builder for element split command
Signature
CreateElementSplitBuilder()
Returns: Return type: NXOpen.CAE.ElementSplitBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementTranslateBuilder¶
-
NodeElementManager.
CreateElementTranslateBuilder
¶ Creates a builder for element translate command
Signature
CreateElementTranslateBuilder()
Returns: Return type: NXOpen.CAE.ElementTranslateBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateElementTypeBuilder¶
-
NodeElementManager.
CreateElementTypeBuilder
¶ Creates a builder for the Element Type Specification block.
Signature
CreateElementTypeBuilder()
Returns: Return type: NXOpen.CAE.ElementTypeBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateGapEadBuilder¶
-
NodeElementManager.
CreateGapEadBuilder
¶ Creates a builder for the Gap EAD block.
Signature
CreateGapEadBuilder()
Returns: Return type: NXOpen.CAE.GapEADBuilder
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateInterpolationEadBuilder¶
-
NodeElementManager.
CreateInterpolationEadBuilder
¶ Creates a builder for the Interpolation EAD block and initializes it with the input element if defined.
Signature
CreateInterpolationEadBuilder(element)
Parameters: element ( NXOpen.CAE.FEElement
) – element to be edited, if None then create a new oneReturns: Return type: NXOpen.CAE.InterpolationEADBuilder
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateLumpedMassEadBuilder¶
-
NodeElementManager.
CreateLumpedMassEadBuilder
¶ Creates a builder for the Lumped Mass EAD block.
Signature
CreateLumpedMassEadBuilder()
Returns: Return type: NXOpen.CAE.LumpedMassEADBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateManualMorphBuilder¶
-
NodeElementManager.
CreateManualMorphBuilder
¶ Creates a builder for Manual Morphing command
Signature
CreateManualMorphBuilder()
Returns: Return type: NXOpen.CAE.ManualMorphBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateManualNodeAssociationBuilder¶
-
NodeElementManager.
CreateManualNodeAssociationBuilder
¶ Creates a builder for manual node association command
Signature
CreateManualNodeAssociationBuilder()
Returns: Return type: NXOpen.CAE.ManualNodeAssociationBuilder
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateMeshFromBoundaryBuilder¶
-
NodeElementManager.
CreateMeshFromBoundaryBuilder
¶ Creates Mesh From Boundary builder.
Signature
CreateMeshFromBoundaryBuilder()
Returns: Return type: NXOpen.CAE.MeshFromBoundaryBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateMorphRevolvedMeshBuilder¶
-
NodeElementManager.
CreateMorphRevolvedMeshBuilder
¶ Creates a
NXOpen.CAE.MorphRevolvedMeshBuilder
Signature
CreateMorphRevolvedMeshBuilder()
Returns: Return type: NXOpen.CAE.MorphRevolvedMeshBuilder
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateMultipleElementCreateBuilder¶
-
NodeElementManager.
CreateMultipleElementCreateBuilder
¶ Creates a builder for the creation of multiple elements.
Signature
CreateMultipleElementCreateBuilder(estimatedNumberOfElements)
Parameters: estimatedNumberOfElements (int) – the estimated number of elements that will be created. It need not be exact. Returns: Return type: NXOpen.CAE.MultipleElementCreateBuilder
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateMultipleNodeCreateBuilder¶
-
NodeElementManager.
CreateMultipleNodeCreateBuilder
¶ Creates a builder for the creation of multiple nodes.
Signature
CreateMultipleNodeCreateBuilder(estimatedNumberOfNodes)
Parameters: estimatedNumberOfNodes (int) – the Estimated number of nodes that will be created. It need not be exact. Returns: Return type: NXOpen.CAE.MultipleNodeCreateBuilder
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodeAlignBuilder¶
-
NodeElementManager.
CreateNodeAlignBuilder
¶ Creates a builder for node align command
Signature
CreateNodeAlignBuilder()
Returns: Return type: NXOpen.CAE.NodeAlignBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodeAssociationBuilder¶
-
NodeElementManager.
CreateNodeAssociationBuilder
¶ Creates a builder for node association command
Signature
CreateNodeAssociationBuilder()
Returns: Return type: NXOpen.CAE.NodeAssociationBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodeCreateBuilder¶
-
NodeElementManager.
CreateNodeCreateBuilder
¶ Creates a builder for node create command
Signature
CreateNodeCreateBuilder()
Returns: Return type: NXOpen.CAE.NodeCreateBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodeDeleteBuilder¶
-
NodeElementManager.
CreateNodeDeleteBuilder
¶ Creates a builder for node delete command
Signature
CreateNodeDeleteBuilder()
Returns: Return type: NXOpen.CAE.NodeDeleteBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodeDissociationBuilder¶
-
NodeElementManager.
CreateNodeDissociationBuilder
¶ Creates a builder for node dissociation command
Signature
CreateNodeDissociationBuilder()
Returns: Return type: NXOpen.CAE.NodeDissociationBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodeModifyLabelBuilder¶
-
NodeElementManager.
CreateNodeModifyLabelBuilder
¶ Creates a builder for node modify label command
Signature
CreateNodeModifyLabelBuilder()
Returns: Return type: NXOpen.CAE.NodeModifyLabelBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodeModifyLocationBuilder¶
-
NodeElementManager.
CreateNodeModifyLocationBuilder
¶ Creates a builder for node modify location command
Signature
CreateNodeModifyLocationBuilder()
Returns: Return type: NXOpen.CAE.NodeModifyLocationBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodeProjectBuilder¶
-
NodeElementManager.
CreateNodeProjectBuilder
¶ Creates a builder for node project command
Signature
CreateNodeProjectBuilder()
Returns: Return type: NXOpen.CAE.NodeProjectBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodeReflectBuilder¶
-
NodeElementManager.
CreateNodeReflectBuilder
¶ Creates a builder for Node reflect command
Signature
CreateNodeReflectBuilder()
Returns: Return type: NXOpen.CAE.NodeReflectBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodeRotateBuilder¶
-
NodeElementManager.
CreateNodeRotateBuilder
¶ Creates a builder for node rotate command
Signature
CreateNodeRotateBuilder()
Returns: Return type: NXOpen.CAE.NodeRotateBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodeTranslateBuilder¶
-
NodeElementManager.
CreateNodeTranslateBuilder
¶ Creates a builder for node translate command
Signature
CreateNodeTranslateBuilder()
Returns: Return type: NXOpen.CAE.NodeTranslateBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodesBetweenNodesBuilder¶
-
NodeElementManager.
CreateNodesBetweenNodesBuilder
¶ Creates a builder for node between nodes command
Signature
CreateNodesBetweenNodesBuilder()
Returns: Return type: NXOpen.CAE.NodesBetweenNodesBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodesOnCurveBuilder¶
-
NodeElementManager.
CreateNodesOnCurveBuilder
¶ Creates a builder for nodes on curve command
Signature
CreateNodesOnCurveBuilder()
Returns: Return type: NXOpen.CAE.NodesOnCurveBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNodesRepositionBuilder¶
-
NodeElementManager.
CreateNodesRepositionBuilder
¶ Creates a builder for repositioning nodes, Use this command when you need to modify many nodes at one time.
Signature
CreateNodesRepositionBuilder()
Returns: Return type: NXOpen.CAE.NodesRepositionBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateOneDimensionalElementSplitBuilder¶
-
NodeElementManager.
CreateOneDimensionalElementSplitBuilder
¶ Creates a builder for one dimensional element split command
Signature
CreateOneDimensionalElementSplitBuilder()
Returns: Return type: NXOpen.CAE.OneDimensionalElementSplitBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateRemoveRibsBuilder¶
-
NodeElementManager.
CreateRemoveRibsBuilder
¶ Creates a builder for remove ribs command
Signature
CreateRemoveRibsBuilder()
Returns: Return type: NXOpen.CAE.RemoveRibsBuilder
New in version NX11.0.0.
License requirements: nx_acoustic_modeling (” NX Acoustic Modeling”)
CreateShellEadBuilder¶
-
NodeElementManager.
CreateShellEadBuilder
¶ Creates a builder for the Shell EAD block.
Signature
CreateShellEadBuilder()
Returns: Return type: NXOpen.CAE.ShellEADBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateSpiderElementBuilder¶
-
NodeElementManager.
CreateSpiderElementBuilder
¶ Creates a builder for spider element command
Signature
CreateSpiderElementBuilder()
Returns: Return type: NXOpen.CAE.SpiderElementBuilder
New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateSpringEadBuilder¶
-
NodeElementManager.
CreateSpringEadBuilder
¶ Creates a builder for the Spring EAD block.
Signature
CreateSpringEadBuilder()
Returns: Return type: NXOpen.CAE.SpringEADBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateSurfaceCoatBuilder¶
-
NodeElementManager.
CreateSurfaceCoatBuilder
¶ Creates a builder for the Surface Coat.
Signature
CreateSurfaceCoatBuilder()
Returns: Return type: NXOpen.CAE.SurfaceCoatBuilder
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateSweepBetweenMeshBuilder¶
-
NodeElementManager.
CreateSweepBetweenMeshBuilder
¶ Creates a builder for Manual Hex Mesh.
Signature
CreateSweepBetweenMeshBuilder()
Returns: Return type: NXOpen.CAE.SweepBetweenMeshBuilder
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateThickenMeshBuilder¶
-
NodeElementManager.
CreateThickenMeshBuilder
¶ Creates a
NXOpen.CAE.ThickenMeshBuilder
Signature
CreateThickenMeshBuilder()
Returns: Return type: NXOpen.CAE.ThickenMeshBuilder
New in version NX11.0.0.
License requirements: nx_acoustic_modeling (” NX Acoustic Modeling”)