SpringEADBuilder Class¶
-
class
NXOpen.CAE.
SpringEADBuilder
¶ Bases:
NXOpen.Builder
This class provides Spring Associated Data Support
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateSpringEadBuilder()
Default values.
Property Value RotationalStiffness.Value 0 (millimeters part), 0 (inches part) StiffnessState Apply TranslationalStiffness.Value 0 (millimeters part), 0 (inches part) New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Elements | Returns the select element operator selects elements |
RotationalStiffness | Returns the expression rotational stiffness operator gets spring rotational stiffness value |
StiffnessState | Returns or sets the stiffness state drives the action upon commit |
Tag | Returns the Tag for this object. |
TranslationalStiffness | Returns the expression stiffness operator gets spring translational stiffness value |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SpringEADBuilderState Enumeration | indicates to apply or clear the stiffness property upon commit |
Property Detail¶
Elements¶
-
SpringEADBuilder.
Elements
¶ Returns the select element operator selects elements
-------------------------------------
Getter Method
Signature
Elements()
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
RotationalStiffness¶
-
SpringEADBuilder.
RotationalStiffness
¶ Returns the expression rotational stiffness operator gets spring rotational stiffness value
-------------------------------------
Getter Method
Signature
RotationalStiffness()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
StiffnessState¶
-
SpringEADBuilder.
StiffnessState
¶ Returns or sets the stiffness state drives the action upon commit
-------------------------------------
Getter Method
Signature
StiffnessState()
Returns: Return type: NXOpen.CAE.SpringEADBuilderState
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
StiffnessState(stiffnessState)
Parameters: stiffnessState ( NXOpen.CAE.SpringEADBuilderState
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
TranslationalStiffness¶
-
SpringEADBuilder.
TranslationalStiffness
¶ Returns the expression stiffness operator gets spring translational stiffness value
-------------------------------------
Getter Method
Signature
TranslationalStiffness()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
SpringEADBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.