ElementConnectivityBuilder Class¶
-
class
NXOpen.CAE.
ElementConnectivityBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ElementConnectivityBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateElementConnectivityBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DeleteOrphan | Returns or sets the delete orphan node flag, telling whether orphan nodes will be deleted |
Element | Returns a selected element whose connectivity is to be modified. |
InNode | Returns the in node which will replace |
Method | Returns or sets an element modification method. |
OutNode | Returns the out node which will be replaced |
SpiderLegNodes | Returns the spider element leg nodes. |
Tag | Returns the Tag for this object. |
Type | Returns or sets a type which indicates whether connectivity is to be modfied for selected element or all attached elements. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ElementConnectivityBuilderMethods Enumeration | Available modify connectivity methods |
ElementConnectivityBuilderTypes Enumeration | Modify connectivity types |
Property Detail¶
DeleteOrphan¶
-
ElementConnectivityBuilder.
DeleteOrphan
¶ Returns or sets the delete orphan node flag, telling whether orphan nodes will be deleted
-------------------------------------
Getter Method
Signature
DeleteOrphan()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeleteOrphan(deleteOrphan)
Parameters: deleteOrphan (bool) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Element¶
-
ElementConnectivityBuilder.
Element
¶ Returns a selected element whose connectivity is to be modified.
-------------------------------------
Getter Method
Signature
Element()
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
InNode¶
-
ElementConnectivityBuilder.
InNode
¶ Returns the in node which will replace
-------------------------------------
Getter Method
Signature
InNode()
Returns: Return type: NXOpen.CAE.SelectFENode
New in version NX5.0.0.
License requirements: None.
Method¶
-
ElementConnectivityBuilder.
Method
¶ Returns or sets an element modification method.
-------------------------------------
Getter Method
Signature
Method()
Returns: Return type: NXOpen.CAE.ElementConnectivityBuilderMethods
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
Method(method)
Parameters: method ( NXOpen.CAE.ElementConnectivityBuilderMethods
) –New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
OutNode¶
-
ElementConnectivityBuilder.
OutNode
¶ Returns the out node which will be replaced
-------------------------------------
Getter Method
Signature
OutNode()
Returns: Return type: NXOpen.CAE.SelectFENode
New in version NX5.0.0.
License requirements: None.
SpiderLegNodes¶
-
ElementConnectivityBuilder.
SpiderLegNodes
¶ Returns the spider element leg nodes.
To delete a leg node, the node should be removed from the list and to add a new leg node, the node is added in the list.
-------------------------------------
Getter Method
Signature
SpiderLegNodes()
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
Type¶
-
ElementConnectivityBuilder.
Type
¶ Returns or sets a type which indicates whether connectivity is to be modfied for selected element or all attached elements.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.CAE.ElementConnectivityBuilderTypes
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.CAE.ElementConnectivityBuilderTypes
) –New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
ElementConnectivityBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.