NodesOnCurveBuilder Class¶
-
class
NXOpen.CAE.
NodesOnCurveBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.NodesOnCurveBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateNodesOnCurveBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Distance | Returns the distance |
Edge | Returns the edge |
Geom | Returns the selected geometry, on which nodes will be created. |
Increment | Returns or sets the increment |
IsClosedCurve | Returns or sets the closedCurve |
Label | Returns or sets the label |
Length | Returns or sets the length |
NumNodes | Returns or sets the num nodes |
PlacementOption | Returns or sets the placement option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
NodesOnCurveBuilderPlacementType Enumeration | the placement type types |
Property Detail¶
Distance¶
-
NodesOnCurveBuilder.
Distance
¶ Returns the distance
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
Edge¶
-
NodesOnCurveBuilder.
Edge
¶ Returns the edge
-------------------------------------
Getter Method
Signature
Edge()
Returns: Return type: NXOpen.CAE.SelectCAEEdge
New in version NX5.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.CAE.NodesOnCurveBuilder.Geom()
instead.License requirements: None.
Geom¶
-
NodesOnCurveBuilder.
Geom
¶ Returns the selected geometry, on which nodes will be created.
Valid selection types are edges, point and curves
NXOpen.CAE.CAEEdge
,NXOpen.Point
,NXOpen.Line
,NXOpen.Edge
,NXOpen.Spline
-------------------------------------
Getter Method
Signature
Geom()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX8.5.0.
License requirements: None.
Increment¶
-
NodesOnCurveBuilder.
Increment
¶ Returns or sets the increment
-------------------------------------
Getter Method
Signature
Increment()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Increment(increment)
Parameters: increment (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
IsClosedCurve¶
-
NodesOnCurveBuilder.
IsClosedCurve
¶ Returns or sets the closedCurve
-------------------------------------
Getter Method
Signature
IsClosedCurve()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsClosedCurve(isClosedCurve)
Parameters: isClosedCurve (bool) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Label¶
-
NodesOnCurveBuilder.
Label
¶ Returns or sets the label
-------------------------------------
Getter Method
Signature
Label()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label(label)
Parameters: label (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Length¶
-
NodesOnCurveBuilder.
Length
¶ Returns or sets the length
-------------------------------------
Getter Method
Signature
Length()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Length(length)
Parameters: length (float) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NumNodes¶
-
NodesOnCurveBuilder.
NumNodes
¶ Returns or sets the num nodes
-------------------------------------
Getter Method
Signature
NumNodes()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumNodes(numNodes)
Parameters: numNodes (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PlacementOption¶
-
NodesOnCurveBuilder.
PlacementOption
¶ Returns or sets the placement option
-------------------------------------
Getter Method
Signature
PlacementOption()
Returns: Return type: NXOpen.CAE.NodesOnCurveBuilderPlacementType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlacementOption(placementOption)
Parameters: placementOption ( NXOpen.CAE.NodesOnCurveBuilderPlacementType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
NodesOnCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.