ElementReflectBuilderLabelType Enumeration

NXOpen.CAE.ElementReflectBuilder.LabelType is an alias for NXOpen.CAE.ElementReflectBuilderLabelType

class NXOpen.CAE.ElementReflectBuilderLabelType

Bases: object

Option to use label/increment or offset

Enum Members

Enum Member Enum Member Description
Label
input label by start number/increment
Offset
by offset
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.