ResultCoordinateSystem Enumeration

NXOpen.CAE.Result.CoordinateSystem is an alias for NXOpen.CAE.ResultCoordinateSystem

class NXOpen.CAE.ResultCoordinateSystem

Bases: object

Coordinate systems

Enum Members

such coordinate systems are defined in the results model; if no material coordinate system is defined NXOpen.CAE.ResultCoordinateSystem.AbsoluteRectangular will be used”

“SelectRectangular”, ” - ” “SelectCylindrical”, ” - ” “SelectSpherical”, ” - “
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.