SimCondition Class¶
-
class
NXOpen.CAE.
SimCondition
¶ Bases:
NXOpen.TaggedObject
This class represents a Condition which defines a state where all or some values of
NXOpen.CAE.SimConditionParam
are known.An instance of this class can be obtained from
NXOpen.CAE.SimConditionSeqMgr
.New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Label | Returns the condition’s label. |
Name | Returns or sets the condition’s name |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetValue | Returns the condition specified parameter value. |
IsValueDefined | Returns if the condition specified parameter value is defined. |
SetValue | Sets the condition specified parameter value. |
Property Detail¶
Label¶
-
SimCondition.
Label
¶ Returns the condition’s label.
Label is unique and greater than zero. It can only be set at creation of a condition and cannot be changed. The label is the key used to locate a specific condition.
-------------------------------------
Getter Method
Signature
Label()
Returns: the label value Return type: int New in version NX9.0.0.
License requirements: None.
Name¶
-
SimCondition.
Name
¶ Returns or sets the condition’s name
-------------------------------------
Getter Method
Signature
Name()
Returns: the name value Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
GetValue¶
-
SimCondition.
GetValue
¶ Returns the condition specified parameter value.
Use the parameter’s object as a key in for the value. Errors out if parameter doesn’t exist. Errors out if value is undefined. Same units as specified
NXOpen.CAE.SimConditionParam
.Signature
GetValue(param)
Parameters: param ( NXOpen.CAE.SimConditionParam
) –Returns: the condition parameter value Return type: float New in version NX9.0.0.
License requirements: None.
IsValueDefined¶
-
SimCondition.
IsValueDefined
¶ Returns if the condition specified parameter value is defined.
Use the parameter’s object as a key in. Errors out if parameter doesn’t exist.
Signature
IsValueDefined(param)
Parameters: param ( NXOpen.CAE.SimConditionParam
) –Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
SetValue¶
-
SimCondition.
SetValue
¶ Sets the condition specified parameter value.
Use the parameter’s object as a key in for the value. Errors out if parameter doesn’t exist. Same units as specified
NXOpen.CAE.SimConditionParam
.Signature
SetValue(param, value)
Parameters: - param (
NXOpen.CAE.SimConditionParam
) – - value (float) –
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- param (