SimConditionSeqMgr Class¶
-
class
NXOpen.CAE.
SimConditionSeqMgr
¶ Bases:
NXOpen.TaggedObject
This is the manager for Condition Sequences. Each Simulation has one manager.
To obtain an instance of this class, use
NXOpen.CAE.SimSimulation.ConditionSeqManager()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ActiveConditionSequence | Returns or sets the currently active Condition Sequence. |
Tag | Returns the Tag for this object. |
ConditionParamCollection |
|
ConditionCollection |
|
ConditionSequenceCollection |
|
Methods¶
Method | Description |
---|---|
ExportFile | Exports a NXOpen.CAE.SimConditionSequence to a file on disk. |
ImportFile | Imports a file from disk to create a NXOpen.CAE.SimConditionSequence . |
IsReferenced | Returns if a NXOpen.CAE.SimCondition is referenced in a NXOpen.CAE.SimConditionSequence @return |
WrapUp | Wrap up all modifications done to NXOpen.CAE.SimConditionSequence , NXOpen.CAE.SimCondition , NXOpen.CAE.SimConditionParam and NXOpen.Expression in order to have all objects in a consistent state. |
Enumerations¶
SimConditionSeqMgrFileFormat Enumeration | Specifies the file format during an import. |
Property Detail¶
ActiveConditionSequence¶
-
SimConditionSeqMgr.
ActiveConditionSequence
¶ Returns or sets the currently active Condition Sequence.
-------------------------------------
Getter Method
Signature
ActiveConditionSequence()
Returns: the active NXOpen.CAE.SimConditionSequence
Return type: NXOpen.CAE.SimConditionSequence
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActiveConditionSequence(sequence)
Parameters: sequence ( NXOpen.CAE.SimConditionSequence
) –New in version NX9.0.0.
License requirements: None.
ConditionParamCollection¶
-
SimConditionSeqMgr.
ConditionParamCollection
¶ Returns the
NXOpen.CAE.SimConditionParamCollection
.Signature
ConditionParamCollection()
New in version NX9.0.0.
Returns: Return type: NXOpen.CAE.SimConditionParamCollection
ConditionCollection¶
-
SimConditionSeqMgr.
ConditionCollection
¶ Returns the
NXOpen.CAE.SimConditionCollection
.Signature
ConditionCollection()
New in version NX9.0.0.
Returns: Return type: NXOpen.CAE.SimConditionCollection
ConditionSequenceCollection¶
-
SimConditionSeqMgr.
ConditionSequenceCollection
¶ Returns the
NXOpen.CAE.SimConditionSequenceCollection
.Signature
ConditionSequenceCollection()
New in version NX9.0.0.
Returns: Return type: NXOpen.CAE.SimConditionSequenceCollection
Method Detail¶
ExportFile¶
-
SimConditionSeqMgr.
ExportFile
¶ Exports a
NXOpen.CAE.SimConditionSequence
to a file on disk.Signature
ExportFile(filename, format)
Parameters: - filename (str) –
- format (
NXOpen.CAE.SimConditionSeqMgrFileFormat
) –
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ImportFile¶
-
SimConditionSeqMgr.
ImportFile
¶ Imports a file from disk to create a
NXOpen.CAE.SimConditionSequence
.Signature
ImportFile(filename, format)
Parameters: - filename (str) –
- format (
NXOpen.CAE.SimConditionSeqMgrFileFormat
) –
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsReferenced¶
-
SimConditionSeqMgr.
IsReferenced
¶ Returns if a
NXOpen.CAE.SimCondition
is referenced in aNXOpen.CAE.SimConditionSequence
Signature
IsReferenced(condition)
Parameters: condition ( NXOpen.CAE.SimCondition
) –Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
WrapUp¶
-
SimConditionSeqMgr.
WrapUp
¶ Wrap up all modifications done to
NXOpen.CAE.SimConditionSequence
,NXOpen.CAE.SimCondition
,NXOpen.CAE.SimConditionParam
andNXOpen.Expression
in order to have all objects in a consistent state.Signature
WrapUp()
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)