LaminateSpreadsheetReportBuilderCoordinateSystemType Enumeration

NXOpen.CAE.LaminateSpreadsheetReportBuilder.CoordinateSystemType is an alias for NXOpen.CAE.LaminateSpreadsheetReportBuilderCoordinateSystemType

class NXOpen.CAE.LaminateSpreadsheetReportBuilderCoordinateSystemType

Bases: object

Coordinate system to use for ply stresses, ply failure indices, ply strength ratios and ply margins of safety calculation.

Enum Members

Enum Member Enum Member Description
Ply
Ply coordinate system
Laminate
Laminate coordinate system
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.