ReassignElementsBuilderElementDimensionOption Enumeration

NXOpen.CAE.ReassignElementsBuilder.ElementDimensionOption is an alias for NXOpen.CAE.ReassignElementsBuilderElementDimensionOption

class NXOpen.CAE.ReassignElementsBuilderElementDimensionOption

Bases: object

Indicates the different element dimensions

Enum Members

Enum Member Enum Member Description
Point
0-d
Beam
1-d
Shell
2-d
Solid
3-d
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.