SimConstraintSetBuilder Class¶
-
class
NXOpen.CAE.
SimConstraintSetBuilder
¶ Bases:
NXOpen.Builder
Represents a
CAE.SimConstraintSetBuilder
builderTo create a new instance of this class, use
NXOpen.CAE.SimSimulation.CreateConstraintSetBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
DescriptorName | Returns the name of the constraint set descriptor |
Label | Returns or sets the label of constraint set |
Name | Returns or sets the name of constraint set |
PropertyTable | Returns the constraint set’s property table |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DescriptorName¶
-
SimConstraintSetBuilder.
DescriptorName
¶ Returns the name of the constraint set descriptor
-------------------------------------
Getter Method
Signature
DescriptorName()
Returns: Return type: str New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Label¶
-
SimConstraintSetBuilder.
Label
¶ Returns or sets the label of constraint set
-------------------------------------
Getter Method
Signature
Label()
Returns: constraint set label Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label(constraintSetLabel)
Parameters: constraintSetLabel (int) – New in version NX11.0.0.
License requirements: None.
Name¶
-
SimConstraintSetBuilder.
Name
¶ Returns or sets the name of constraint set
-------------------------------------
Getter Method
Signature
Name()
Returns: constraint set name Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(constraintSetName)
Parameters: constraintSetName (str) – New in version NX11.0.0.
License requirements: None.
PropertyTable¶
-
SimConstraintSetBuilder.
PropertyTable
¶ Returns the constraint set’s property table
-------------------------------------
Getter Method
Signature
PropertyTable()
Returns: constraint set property table Return type: NXOpen.CAE.PropertyTable
New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SimConstraintSetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.