ManualMorphBuilderMapMethod Enumeration¶
NXOpen.CAE.ManualMorphBuilder.MapMethod is an alias for NXOpen.CAE.ManualMorphBuilderMapMethod
-
class
NXOpen.CAE.
ManualMorphBuilderMapMethod
¶ Bases:
object
Represents the chosen type to apply node mapping on selected geometry.
For example the nearest point or along specifed vector.
Enum Members
Enum Member Enum Member Description NearestPoint AlongVector UniformAcrossEdge KeepSourceBias BasedOnEdgeNodeMovement AlongElementNormal -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-