MeshPointCollection Class¶
-
class
NXOpen.CAE.
MeshPointCollection
¶ Bases:
object
Provides methods for managing constraints
NXOpen.CAE.MeshPoint
in a sim part.Iterating this collection only returns live uncondemned objects contained in the owning part of the collection. Note that
NXOpen.CAE.MeshPoint
is a smart object and many smart objects are condemned as they only exist to support other objects and are not displayed. Condemned objects will be deleted when their references go away. To obtain an instance of this class, refer toNXOpen.CAE.FemPart
New in version NX5.0.2.
Methods¶
Method | Description |
---|---|
CreateMeshpointConicCenterBuilder | Creates a NXOpen.CAE.MeshPointConicCenterBuilder object. |
CreateMeshpointExistingPointBuilder | Creates a NXOpen.CAE.MeshPointExistingPointBuilder object. |
CreateMeshpointMultipleOnCurveBuilder | Creates a NXOpen.CAE.MeshPointMultipleOnCurveBuilder object. |
CreateMeshpointOnCurveBuilder | Creates a NXOpen.CAE.MeshPointOnCurveBuilder object. |
CreateMeshpointOnFaceBuilder | Creates a NXOpen.CAE.MeshPointOnFaceBuilder object. |
CreateMeshpointProjectBuilder | Creates a NXOpen.CAE.MeshPointProjectBuilder object. |
FindObject | Finds the NXOpen.CAE.MeshPoint with the given identifier as recorded in a journal. |
Method Detail¶
CreateMeshpointConicCenterBuilder¶
-
MeshPointCollection.
CreateMeshpointConicCenterBuilder
¶ Creates a
NXOpen.CAE.MeshPointConicCenterBuilder
object.Signature
CreateMeshpointConicCenterBuilder()
Returns: Return type: NXOpen.CAE.MeshPointConicCenterBuilder
New in version NX5.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateMeshpointExistingPointBuilder¶
-
MeshPointCollection.
CreateMeshpointExistingPointBuilder
¶ Creates a
NXOpen.CAE.MeshPointExistingPointBuilder
object.Signature
CreateMeshpointExistingPointBuilder()
Returns: Return type: NXOpen.CAE.MeshPointExistingPointBuilder
New in version NX5.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateMeshpointMultipleOnCurveBuilder¶
-
MeshPointCollection.
CreateMeshpointMultipleOnCurveBuilder
¶ Creates a
NXOpen.CAE.MeshPointMultipleOnCurveBuilder
object.Signature
CreateMeshpointMultipleOnCurveBuilder()
Returns: Return type: NXOpen.CAE.MeshPointMultipleOnCurveBuilder
New in version NX5.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateMeshpointOnCurveBuilder¶
-
MeshPointCollection.
CreateMeshpointOnCurveBuilder
¶ Creates a
NXOpen.CAE.MeshPointOnCurveBuilder
object.Signature
CreateMeshpointOnCurveBuilder()
Returns: Return type: NXOpen.CAE.MeshPointOnCurveBuilder
New in version NX5.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateMeshpointOnFaceBuilder¶
-
MeshPointCollection.
CreateMeshpointOnFaceBuilder
¶ Creates a
NXOpen.CAE.MeshPointOnFaceBuilder
object.Signature
CreateMeshpointOnFaceBuilder()
Returns: Return type: NXOpen.CAE.MeshPointOnFaceBuilder
New in version NX5.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateMeshpointProjectBuilder¶
-
MeshPointCollection.
CreateMeshpointProjectBuilder
¶ Creates a
NXOpen.CAE.MeshPointProjectBuilder
object.Signature
CreateMeshpointProjectBuilder()
Returns: Return type: NXOpen.CAE.MeshPointProjectBuilder
New in version NX5.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
FindObject¶
-
MeshPointCollection.
FindObject
¶ Finds the
NXOpen.CAE.MeshPoint
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the MeshPoint you want Returns: Return type: NXOpen.CAE.MeshPoint
New in version NX5.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)