CaeGroupElementSubType Enumeration¶
-
class
NXOpen.CAE.
CaeGroupElementSubType
¶ Bases:
object
Used to specify the sub type of selected objects e.
g face of an element, edge of an element ..etc Enum Members
Enum Member Enum Member Description Face sub type is element faceEdge sub type is element edge-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-