ResultsCombinationBuilderOutput Enumeration

NXOpen.CAE.ResultsCombinationBuilder.Output is an alias for NXOpen.CAE.ResultsCombinationBuilderOutput

class NXOpen.CAE.ResultsCombinationBuilderOutput

Bases: object

output types

Enum Members

Enum Member Enum Member Description
ExportResultFile  
CreateField  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.