FeatureElemEdgeMethod Class

class NXOpen.CAE.FeatureElemEdgeMethod

Bases: NXOpen.SelectionMethod

Represents the output from the feature element edge smart selector method

To obtain an instance of this class use CAE::SmartSelectionManager

New in version NX6.0.0.

Methods

Method Description
Dispose Frees the object from memory.
GetElementEdges Returns the resultant element edges @return
GetSelectedObjects Returns the objects selected by this NXOpen.SelectionMethod.

Method Detail

Dispose

FeatureElemEdgeMethod.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX6.0.0.

License requirements: None.

GetElementEdges

FeatureElemEdgeMethod.GetElementEdges

Returns the resultant element edges

Signature GetElementEdges()

Returns:
Return type:list of NXOpen.CAE.SetObject

New in version NX6.0.4.

License requirements: None.