NodesBetweenNodesBuilderTypeEnum Enumeration

NXOpen.CAE.NodesBetweenNodesBuilder.TypeEnum is an alias for NXOpen.CAE.NodesBetweenNodesBuilderTypeEnum

class NXOpen.CAE.NodesBetweenNodesBuilderTypeEnum

Bases: object

the method of creation of node

Enum Members

Enum Member Enum Member Description
NodesBetweenTwoNodes
Between two nodes
NodeAtCenterOfThreeNodes
At the center of imaginary circle defined by 3 nodes
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.