LaminateDynamicEventCollection Class

class NXOpen.CAE.LaminateDynamicEventCollection

Bases: object

Represents a collection of laminate dynamic events

To obtain an instance of this class, refer to NXOpen.CAE.LaminateDynamicSim

New in version NX9.0.0.

Methods

Method Description
CloneDynamicEvent Clones the laminate dynamic event
CreateRandomEventBuilder Creates a builder for the laminate random event.
CreateSineEventBuilder Creates a builder for the laminate sine event.
Delete Deletes the laminate dynamic event
FindObject Finds a laminate dynamic event with the specified name @return Laminate Dynamic Event found

Method Detail

CloneDynamicEvent

LaminateDynamicEventCollection.CloneDynamicEvent

Clones the laminate dynamic event

Signature CloneDynamicEvent(dynamicEvent)

Parameters:dynamicEvent (NXOpen.CAE.LaminateDynamicEvent) – Laminate dynamic event to be cloned

New in version NX9.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

CreateRandomEventBuilder

LaminateDynamicEventCollection.CreateRandomEventBuilder

Creates a builder for the laminate random event.

Signature CreateRandomEventBuilder(laminateRandomEventTag)

Parameters:laminateRandomEventTag (NXOpen.CAE.LaminateRandomEvent) – The event.
Returns:
Return type:NXOpen.CAE.LaminateRandomEventBuilder

New in version NX9.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

CreateSineEventBuilder

LaminateDynamicEventCollection.CreateSineEventBuilder

Creates a builder for the laminate sine event.

Signature CreateSineEventBuilder(laminateSineEventTag)

Parameters:laminateSineEventTag (NXOpen.CAE.LaminateSineEvent) – The event.
Returns:
Return type:NXOpen.CAE.LaminateSineEventBuilder

New in version NX10.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

Delete

LaminateDynamicEventCollection.Delete

Deletes the laminate dynamic event

Signature Delete(dynamicEvent)

Parameters:dynamicEvent (NXOpen.CAE.LaminateDynamicEvent) – Laminate dynamic event to be deleted

New in version NX9.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)

FindObject

LaminateDynamicEventCollection.FindObject

Finds a laminate dynamic event with the specified name

Signature FindObject(name)

Parameters:name (str) – Laminate Dynamic Event name to be found
Returns:Laminate Dynamic Event found
Return type:NXOpen.CAE.LaminateDynamicEvent

New in version NX9.0.0.

License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)