LaminateSineEventBuilder Class¶
-
class
NXOpen.CAE.
LaminateSineEventBuilder
¶ Bases:
NXOpen.CAE.LaminateDynamicEventBuilder
Represents a
NXOpen.CAE.LaminateSineEvent
builderTo create a new instance of this class, use
NXOpen.CAE.LaminateDynamicEventCollection.CreateSineEventBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
AdditionalFrequenciesBreakPoints | Returns or sets the option to consider break points |
AdditionalFrequenciesUnits | Returns or sets the option to consider break points |
DynamicEventName | Returns or sets the event name |
ExcitationCsys | Returns or sets the excitation coordinate system |
ExcitationSelectedAxis | Returns or sets the excitation axis |
IntermediateFrequenciesBetweenOption | Returns or sets the intermediate in between frequencies option |
IntermediateFrequenciesCluster | Returns or sets the intermediate in between frequencies number of excitations |
IntermediateFrequenciesEnable | Returns or sets the intermediate frequencies control |
IntermediateFrequenciesIncludeNatFreq | Returns or sets the option to include the natural frequencis in the intermediate frequencies with the linear and logarithmic options |
IntermediateFrequenciesNumExcitations | Returns or sets the intermediate in between frequencies number of excitations |
IntermediateFrequenciesNumIncrements | Returns or sets the intermediate frequencies number of increments for linear and logarithmic options |
IntermediateFrequenciesOption | Returns or sets the intermediate frequencies option |
LowerBoundFrequency | Returns or sets the lower bound freq |
NastranBasicCsys | Returns or sets the nastran basic |
NaturalFrequenciesChoice | Returns or sets the natural frequencies selection option |
NaturalFrequenciesEnable | Returns or sets the natural frequencies option |
ReferenceType | Returns or sets the reference type |
Tag | Returns the Tag for this object. |
UpperBoundFrequency | Returns or sets the upper bound freq |
UserFunction | Returns or sets the function. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOutputRequestObject | Get the output request. |
SelectModes | Sets the a mode property selection |
SetAdditionalFrequencies | Sets the additional frequencies values |
SetOutputRequestObject | Set the output request. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LaminateSineEventBuilderAdditionalFrequeciesUnitsEnum Enumeration | The additional frequencies units |
LaminateSineEventBuilderIntermediateFrequeciesBetweenEnum Enumeration | The intermediate in between frequencies increment option |
LaminateSineEventBuilderIntermediateFrequeciesEnum Enumeration | The intermediate frequencies options |
LaminateSineEventBuilderNaturalFrequeciesEnum Enumeration | The reference enum. |
Property Detail¶
AdditionalFrequenciesBreakPoints¶
-
LaminateSineEventBuilder.
AdditionalFrequenciesBreakPoints
¶ Returns or sets the option to consider break points
-------------------------------------
Getter Method
Signature
AdditionalFrequenciesBreakPoints()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdditionalFrequenciesBreakPoints(additionalFrequenciesBreakPoints)
Parameters: additionalFrequenciesBreakPoints (bool) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
AdditionalFrequenciesUnits¶
-
LaminateSineEventBuilder.
AdditionalFrequenciesUnits
¶ Returns or sets the option to consider break points
-------------------------------------
Getter Method
Signature
AdditionalFrequenciesUnits()
Returns: Return type: NXOpen.CAE.LaminateSineEventBuilderAdditionalFrequeciesUnitsEnum
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdditionalFrequenciesUnits(additionalFrequenciesUnits)
Parameters: additionalFrequenciesUnits ( NXOpen.CAE.LaminateSineEventBuilderAdditionalFrequeciesUnitsEnum
) –New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
IntermediateFrequenciesBetweenOption¶
-
LaminateSineEventBuilder.
IntermediateFrequenciesBetweenOption
¶ Returns or sets the intermediate in between frequencies option
-------------------------------------
Getter Method
Signature
IntermediateFrequenciesBetweenOption()
Returns: Return type: NXOpen.CAE.LaminateSineEventBuilderIntermediateFrequeciesBetweenEnum
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IntermediateFrequenciesBetweenOption(intermediateFrequenciesBetweenOption)
Parameters: intermediateFrequenciesBetweenOption ( NXOpen.CAE.LaminateSineEventBuilderIntermediateFrequeciesBetweenEnum
) –New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
IntermediateFrequenciesCluster¶
-
LaminateSineEventBuilder.
IntermediateFrequenciesCluster
¶ Returns or sets the intermediate in between frequencies number of excitations
-------------------------------------
Getter Method
Signature
IntermediateFrequenciesCluster()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IntermediateFrequenciesCluster(intermediateFrequenciesCluster)
Parameters: intermediateFrequenciesCluster (float) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
IntermediateFrequenciesEnable¶
-
LaminateSineEventBuilder.
IntermediateFrequenciesEnable
¶ Returns or sets the intermediate frequencies control
-------------------------------------
Getter Method
Signature
IntermediateFrequenciesEnable()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IntermediateFrequenciesEnable(intermediateFrequenciesEnable)
Parameters: intermediateFrequenciesEnable (bool) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
IntermediateFrequenciesIncludeNatFreq¶
-
LaminateSineEventBuilder.
IntermediateFrequenciesIncludeNatFreq
¶ Returns or sets the option to include the natural frequencis in the intermediate frequencies with the linear and logarithmic options
-------------------------------------
Getter Method
Signature
IntermediateFrequenciesIncludeNatFreq()
Returns: Return type: bool New in version NX10.0.0.
Deprecated since version NX11.0.0: This function has no replacement. The IntermediateFrequenciesIncludeNatFreq property is simply not supported by the Sine Event solver and has never been. This parameter is useless.
License requirements: None.
-------------------------------------
Setter Method
Signature
IntermediateFrequenciesIncludeNatFreq(intermediateFrequenciesIncludeNatFreq)
Parameters: intermediateFrequenciesIncludeNatFreq (bool) – New in version NX10.0.0.
Deprecated since version NX11.0.0: This function has no replacement. The IntermediateFrequenciesIncludeNatFreq property is simply not supported by the Sine Event solver and has never been. This parameter is useless.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
IntermediateFrequenciesNumExcitations¶
-
LaminateSineEventBuilder.
IntermediateFrequenciesNumExcitations
¶ Returns or sets the intermediate in between frequencies number of excitations
-------------------------------------
Getter Method
Signature
IntermediateFrequenciesNumExcitations()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IntermediateFrequenciesNumExcitations(intermediateFrequenciesNumExcitations)
Parameters: intermediateFrequenciesNumExcitations (int) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
IntermediateFrequenciesNumIncrements¶
-
LaminateSineEventBuilder.
IntermediateFrequenciesNumIncrements
¶ Returns or sets the intermediate frequencies number of increments for linear and logarithmic options
-------------------------------------
Getter Method
Signature
IntermediateFrequenciesNumIncrements()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IntermediateFrequenciesNumIncrements(intermediateFrequenciesNumIncrements)
Parameters: intermediateFrequenciesNumIncrements (int) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
IntermediateFrequenciesOption¶
-
LaminateSineEventBuilder.
IntermediateFrequenciesOption
¶ Returns or sets the intermediate frequencies option
-------------------------------------
Getter Method
Signature
IntermediateFrequenciesOption()
Returns: Return type: NXOpen.CAE.LaminateSineEventBuilderIntermediateFrequeciesEnum
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IntermediateFrequenciesOption(intermediateFrequenciesOption)
Parameters: intermediateFrequenciesOption ( NXOpen.CAE.LaminateSineEventBuilderIntermediateFrequeciesEnum
) –New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
NaturalFrequenciesChoice¶
-
LaminateSineEventBuilder.
NaturalFrequenciesChoice
¶ Returns or sets the natural frequencies selection option
-------------------------------------
Getter Method
Signature
NaturalFrequenciesChoice()
Returns: Return type: NXOpen.CAE.LaminateSineEventBuilderNaturalFrequeciesEnum
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NaturalFrequenciesChoice(naturalFrequenciesChoice)
Parameters: naturalFrequenciesChoice ( NXOpen.CAE.LaminateSineEventBuilderNaturalFrequeciesEnum
) –New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
NaturalFrequenciesEnable¶
-
LaminateSineEventBuilder.
NaturalFrequenciesEnable
¶ Returns or sets the natural frequencies option
-------------------------------------
Getter Method
Signature
NaturalFrequenciesEnable()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NaturalFrequenciesEnable(naturalFrequenciesEnable)
Parameters: naturalFrequenciesEnable (bool) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Method Detail¶
SelectModes¶
-
LaminateSineEventBuilder.
SelectModes
¶ Sets the a mode property selection
Signature
SelectModes(selectedModes)
Parameters: selectedModes (list of NXOpen.CAE.LaminateModeProperty
) –New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SetAdditionalFrequencies¶
-
LaminateSineEventBuilder.
SetAdditionalFrequencies
¶ Sets the additional frequencies values
Signature
SetAdditionalFrequencies(additionalFrequencies)
Parameters: additionalFrequencies (list of float) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Validate¶
-
LaminateSineEventBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.