LaminateDynamicEventBuilder Class¶
-
class
NXOpen.CAE.
LaminateDynamicEventBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.LaminateDynamicEvent
builderThis is an abstract class.
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
DynamicEventName | Returns or sets the event name |
ExcitationCsys | Returns or sets the excitation coordinate system |
ExcitationSelectedAxis | Returns or sets the excitation axis |
LowerBoundFrequency | Returns or sets the lower bound freq |
NastranBasicCsys | Returns or sets the nastran basic |
ReferenceType | Returns or sets the reference type |
Tag | Returns the Tag for this object. |
UpperBoundFrequency | Returns or sets the upper bound freq |
UserFunction | Returns or sets the function. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOutputRequestObject | Get the output request. |
SetOutputRequestObject | Set the output request. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LaminateDynamicEventBuilderExcitationSelectedAxisEnum Enumeration | The excitation axis enum. |
LaminateDynamicEventBuilderReferenceTypeEnum Enumeration | The reference enum. |
Property Detail¶
DynamicEventName¶
-
LaminateDynamicEventBuilder.
DynamicEventName
¶ Returns or sets the event name
-------------------------------------
Getter Method
Signature
DynamicEventName()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DynamicEventName(dynamicEventName)
Parameters: dynamicEventName (str) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ExcitationCsys¶
-
LaminateDynamicEventBuilder.
ExcitationCsys
¶ Returns or sets the excitation coordinate system
-------------------------------------
Getter Method
Signature
ExcitationCsys()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExcitationCsys(excitationCsys)
Parameters: excitationCsys ( NXOpen.CoordinateSystem
) –New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ExcitationSelectedAxis¶
-
LaminateDynamicEventBuilder.
ExcitationSelectedAxis
¶ Returns or sets the excitation axis
-------------------------------------
Getter Method
Signature
ExcitationSelectedAxis()
Returns: Return type: NXOpen.CAE.LaminateDynamicEventBuilderExcitationSelectedAxisEnum
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExcitationSelectedAxis(excitationSelectedAxis)
Parameters: excitationSelectedAxis ( NXOpen.CAE.LaminateDynamicEventBuilderExcitationSelectedAxisEnum
) –New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
LowerBoundFrequency¶
-
LaminateDynamicEventBuilder.
LowerBoundFrequency
¶ Returns or sets the lower bound freq
-------------------------------------
Getter Method
Signature
LowerBoundFrequency()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowerBoundFrequency(lowerBoundFrequency)
Parameters: lowerBoundFrequency (float) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
NastranBasicCsys¶
-
LaminateDynamicEventBuilder.
NastranBasicCsys
¶ Returns or sets the nastran basic
-------------------------------------
Getter Method
Signature
NastranBasicCsys()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NastranBasicCsys(nastranBasicCsys)
Parameters: nastranBasicCsys (bool) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ReferenceType¶
-
LaminateDynamicEventBuilder.
ReferenceType
¶ Returns or sets the reference type
-------------------------------------
Getter Method
Signature
ReferenceType()
Returns: Return type: NXOpen.CAE.LaminateDynamicEventBuilderReferenceTypeEnum
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceType(referenceType)
Parameters: referenceType ( NXOpen.CAE.LaminateDynamicEventBuilderReferenceTypeEnum
) –New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
UpperBoundFrequency¶
-
LaminateDynamicEventBuilder.
UpperBoundFrequency
¶ Returns or sets the upper bound freq
-------------------------------------
Getter Method
Signature
UpperBoundFrequency()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperBoundFrequency(upperBoundFrequency)
Parameters: upperBoundFrequency (float) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
UserFunction¶
-
LaminateDynamicEventBuilder.
UserFunction
¶ Returns or sets the function.
-------------------------------------
Getter Method
Signature
UserFunction()
Returns: Return type: NXOpen.TaggedObject
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserFunction(userFunction)
Parameters: userFunction ( NXOpen.TaggedObject
) –New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Method Detail¶
GetOutputRequestObject¶
-
LaminateDynamicEventBuilder.
GetOutputRequestObject
¶ Get the output request.
Signature
GetOutputRequestObject()
Returns: Return type: NXOpen.CAE.ModelingObjectPropertyTable
New in version NX10.0.0.
License requirements: None.
SetOutputRequestObject¶
-
LaminateDynamicEventBuilder.
SetOutputRequestObject
¶ Set the output request.
Signature
SetOutputRequestObject(ssmo)
Parameters: ssmo ( NXOpen.CAE.ModelingObjectPropertyTable
) –New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Validate¶
-
LaminateDynamicEventBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.