LaminateSineEventBuilderIntermediateFrequeciesBetweenEnum Enumeration

NXOpen.CAE.LaminateSineEventBuilder.IntermediateFrequeciesBetweenEnum is an alias for NXOpen.CAE.LaminateSineEventBuilderIntermediateFrequeciesBetweenEnum

class NXOpen.CAE.LaminateSineEventBuilderIntermediateFrequeciesBetweenEnum

Bases: object

The intermediate in between frequencies increment option

Enum Members

Enum Member Enum Member Description
Linear
Linear increments
Logarithmic
Logarithmic increments
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.