ElementExtrudeBuilderMethodType Enumeration

NXOpen.CAE.ElementExtrudeBuilder.MethodType is an alias for NXOpen.CAE.ElementExtrudeBuilderMethodType

class NXOpen.CAE.ElementExtrudeBuilderMethodType

Bases: object

Extrusion method

Enum Members

Enum Member Enum Member Description
Vector
along vector
Path
along path
ProjSurface
project to surface
ElemNormal
along element normal
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.