CADModeling Class¶
-
class
NXOpen.CAE.
CADModeling
¶ Bases:
object
The CADModeling class provides method to create cad face using polygon face
To obtain an instance of this class, refer to
NXOpen.CAE.FemPart
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
CreateCurvesFromPolygonFace | CREATE curves from polygon face in part |
CreateSurfaceFromPolygonFace | CREATE cad surface from polygon face in part @return surface feature |
Method Detail¶
CreateCurvesFromPolygonFace¶
-
CADModeling.
CreateCurvesFromPolygonFace
¶ CREATE curves from polygon face in part
Signature
CreateCurvesFromPolygonFace(cadPart, polygonFace)
Parameters: - cadPart (
NXOpen.Part
) – the target cad part - polygonFace (
NXOpen.CAE.CAEFace
) – the polygon face
Returns: line segments
Return type: list of
NXOpen.TaggedObject
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- cadPart (
CreateSurfaceFromPolygonFace¶
-
CADModeling.
CreateSurfaceFromPolygonFace
¶ CREATE cad surface from polygon face in part
Signature
CreateSurfaceFromPolygonFace(cadPart, polygonFace)
Parameters: - cadPart (
NXOpen.Part
) – the target cad part - polygonFace (
NXOpen.CAE.CAEFace
) – the polygon face
Returns: surface feature
Return type: New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- cadPart (