BeamEADBuilderState Enumeration

NXOpen.CAE.BeamEADBuilder.State is an alias for NXOpen.CAE.BeamEADBuilderState

class NXOpen.CAE.BeamEADBuilderState

Bases: object

indicates to ignore, apply or clear the state property upon commit

Enum Members

Enum Member Enum Member Description
Ignore
ignore the property
Apply
apply the property
Clear
clear the property
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.