ResultsReductionBuilder Class¶
-
class
NXOpen.CAE.
ResultsReductionBuilder
¶ Bases:
NXOpen.CAE.ResultsManipulationBuilder
Represents a
NXOpen.CAE.ResultsReductionBuilder
To obtain an instance of this class use
NXOpen.Session.ResultManager()
.New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAction | The action |
SetAppendMethod | The append method if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult |
SetCompanionResultName | The companion result name if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult |
SetCompanionResultReference | The companion Result Reference if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult |
SetCompanionSolution | The companion solution if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult |
SetCreateSolution | Specifies whether to create an imported solution |
SetDependentDomainName | Set Dependent Domain Name |
SetElementValueAtNode | Set element value to be used at a node |
SetEvaluationErrorOption | Set evaluation error option |
SetFieldName | Set field Name to be created |
SetFormula | The formula |
SetImportResult | Import the result immediately |
SetImportedSolutionName | The imported solution name if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateImportedSolution |
SetIncludeModel | Include nodes and elements |
SetIncompatibleResultsOption | Set incompatible results option |
SetIndependentDomainName | Set Independent Domain Name |
SetLoadcaseName | The load case name |
SetNoDataOption | Set no data option |
SetOutput | Set output type from result reduction |
SetOutputFile | The output file |
SetOutputName | The output name |
SetOutputQuantity | The output quantity |
SetOutputResultType | The result output type |
SetResultTypeName | Set result type name that will be displayed in postview |
SetResultUnit | Set result unit for given result type/dependent field variable type |
SetResults | The result types |
SetUnitsSystem | The units system |
SetUnitsSystemResult | The result to copy the units system from |
SetUserDefinedUnitsSystem | The user-defined units system |
SetViewIndexForPostView | Set view index where postview will be created |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ResultsReductionBuilderEvaluationError Enumeration | evaluation error options |
ResultsReductionBuilderIncompatibleResults Enumeration | Incompatible results options |
ResultsReductionBuilderNoData Enumeration | No data options |
ResultsReductionBuilderOutput Enumeration | output types |
Method Detail¶
SetDependentDomainName¶
-
ResultsReductionBuilder.
SetDependentDomainName
¶ Set Dependent Domain Name
Signature
SetDependentDomainName(domainName)
Parameters: domainName (str) – New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetElementValueAtNode¶
-
ResultsReductionBuilder.
SetElementValueAtNode
¶ Set element value to be used at a node
Signature
SetElementValueAtNode(value)
Parameters: value ( NXOpen.CAE.ResultsManipulationBuilderElementValueAtNode
) –New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetEvaluationErrorOption¶
-
ResultsReductionBuilder.
SetEvaluationErrorOption
¶ Set evaluation error option
Signature
SetEvaluationErrorOption(evaluationErrorOption)
Parameters: evaluationErrorOption ( NXOpen.CAE.ResultsReductionBuilderEvaluationError
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetFieldName¶
-
ResultsReductionBuilder.
SetFieldName
¶ Set field Name to be created
Signature
SetFieldName(fieldName)
Parameters: fieldName (str) – New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetFormula¶
-
ResultsReductionBuilder.
SetFormula
¶ The formula
Signature
SetFormula(formula)
Parameters: formula (str) – set formula New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetIncompatibleResultsOption¶
-
ResultsReductionBuilder.
SetIncompatibleResultsOption
¶ Set incompatible results option
Signature
SetIncompatibleResultsOption(incompatibleResultsOption)
Parameters: incompatibleResultsOption ( NXOpen.CAE.ResultsReductionBuilderIncompatibleResults
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetIndependentDomainName¶
-
ResultsReductionBuilder.
SetIndependentDomainName
¶ Set Independent Domain Name
Signature
SetIndependentDomainName(domainName)
Parameters: domainName (str) – New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetNoDataOption¶
-
ResultsReductionBuilder.
SetNoDataOption
¶ Set no data option
Signature
SetNoDataOption(noDataOption)
Parameters: noDataOption ( NXOpen.CAE.ResultsReductionBuilderNoData
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetOutput¶
-
ResultsReductionBuilder.
SetOutput
¶ Set output type from result reduction
Signature
SetOutput(output)
Parameters: output ( NXOpen.CAE.ResultsReductionBuilderOutput
) –New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResultTypeName¶
-
ResultsReductionBuilder.
SetResultTypeName
¶ Set result type name that will be displayed in postview
Signature
SetResultTypeName(resultTypeName)
Parameters: resultTypeName (str) – New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResultUnit¶
-
ResultsReductionBuilder.
SetResultUnit
¶ Set result unit for given result type/dependent field variable type
Signature
SetResultUnit(unit)
Parameters: unit ( NXOpen.Unit
) –New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResults¶
-
ResultsReductionBuilder.
SetResults
¶ The result types
Signature
SetResults(results, parameters, names)
Parameters: - results (list of
NXOpen.CAE.Result
) – set results - parameters (list of
NXOpen.CAE.ResultParameters
) – set result parameters - names (list of str) – set result names
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- results (list of
SetViewIndexForPostView¶
-
ResultsReductionBuilder.
SetViewIndexForPostView
¶ Set view index where postview will be created
Signature
SetViewIndexForPostView(viewIndex)
Parameters: viewIndex (int) – New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
ResultsReductionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.