FeatureEdgeNodeMethod Class

class NXOpen.CAE.FeatureEdgeNodeMethod

Bases: NXOpen.SelectionMethod

Represents the output from the feature edge node smart selector method

To obtain an instance of this class use CAE::SmartSelectionManager

New in version NX6.0.0.

Methods

Method Description
Dispose Frees the object from memory.
GetNodes Returns the resultant nodes @return Resultant nodes
GetSelectedObjects Returns the objects selected by this NXOpen.SelectionMethod.

Method Detail

Dispose

FeatureEdgeNodeMethod.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX6.0.0.

License requirements: None.

GetNodes

FeatureEdgeNodeMethod.GetNodes

Returns the resultant nodes

Signature GetNodes()

Returns:Resultant nodes
Return type:list of NXOpen.CAE.FENode

New in version NX6.0.4.

License requirements: None.