ResultTensorDerivedAbsolute Enumeration

NXOpen.CAE.Result.TensorDerivedAbsolute is an alias for NXOpen.CAE.ResultTensorDerivedAbsolute

class NXOpen.CAE.ResultTensorDerivedAbsolute

Bases: object

This enumeration defines the methods that can be used when calculating absolute values for the following derived components of NXOpen.CAE.ResultDataType.Tensor NXOpen.CAE.ResultComponent.Determinant, NXOpen.CAE.ResultComponent.Mean, NXOpen.CAE.ResultComponent.MaximumShear, NXOpen.CAE.ResultComponent.MinimumPrincipal, NXOpen.CAE.ResultComponent.MiddlePrincipal, NXOpen.CAE.ResultComponent.MaximumPrincipal, NXOpen.CAE.ResultComponent.Octahedral

NXOpen.CAE.ResultTensorDerivedAbsolute.AllComponents will make all tensor primary components (XX, YY, ZZ, XY, YZ, ZX) to absolute and then calculate derived component.

NXOpen.CAE.ResultTensorDerivedAbsolute.DerivedComponent is absolute value of derived component without changing primary components.

Enum Members

Enum Member Enum Member Description
AllComponents
Absolute of primary components first
DerivedComponent
Absolute of current derived components
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.