ResultComponent Enumeration¶
NXOpen.CAE.Result.Component is an alias for NXOpen.CAE.ResultComponent
-
class
NXOpen.CAE.
ResultComponent
¶ Bases:
object
Result components
Enum Members
Enum Member Enum Member Description Scalar X Y Z Magnitude Xx Yy Zz Xy Yz Zx Determinant Mean MaximumShear MinimumPrincipal MiddlePrincipal MaximumPrincipal Octahedral VonMises MembraneXX MembraneYY MembraneXY BendingXX BendingYY BendingXY ShearYZ ShearXZ Axial BendingS BendingT Torsion ShearS ShearT SpringDashpotForce No longer used; it meansNXOpen.CAE.ResultComponent.SpringDashpotForceX
in new formatSpringDashpotForceX SpringDashpotForceY SpringDashpotForceZ SpringDashpotMomentX SpringDashpotMomentY SpringDashpotMomentZ Scalar1 Scalar2 Scalar3 Scalar4 Scalar5 Scalar6 Scalar7 Scalar8 Scalar9 Scalar10 Scalar11 Scalar12 WorstPrincipal -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-