LaminateGlobalLayup Class¶
-
class
NXOpen.CAE.
LaminateGlobalLayup
¶ Bases:
NXOpen.NXObject
Represent a global layup in the ply based modeling.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ActiveStatus | Returns or sets the global layup active status |
FiberOrientationOptions | Returns the fiber orientation options |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Label | Returns or sets the global layup label |
Name | Returns or sets the global layup name |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
StackingRecipe | Returns or sets the global layup stacking recipe |
Tag | Returns the Tag for this object. |
PlyGroups |
|
Methods¶
Method | Description |
---|---|
AutogroupByMaterials | Create groups for materials |
ClearLayup | Removes all the ply groups and plies from the global layup |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
CreateFiberOrientationOptionsBuilder | Creates a NXOpen.CAE.LaminateFiberOrientationOptionsBuilder @return |
CreateLockAngleBuilder | Creates a NXOpen.CAE.LaminateLockAngleBuilder @return |
DefineSymPlyidRange | Defines the range of id to be used for symmetric and repeated plies. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
ExportDrapingDomainAsGroups | Exports draping domain to a group |
ExportDrapingResults | Exports draping results to a csv file. |
ExportLayup | Export simple layup definition to a csv file. |
ExportPliesToFibersim | Exports ply definitions to FiberSim using the hdf5 file format. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Information | Display global layup information |
Prints a representation of this object to the system log file. | |
RefreshLinkedGroups | Refresh the global layup linked ply group state |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
UpdateDraping | Compute draping for all the plies under this global layup. |
Enumerations¶
LaminateGlobalLayupStackingRecipeType Enumeration | Used to specify the stacking recipe of the global layup |
Property Detail¶
ActiveStatus¶
-
LaminateGlobalLayup.
ActiveStatus
¶ Returns or sets the global layup active status
-------------------------------------
Getter Method
Signature
ActiveStatus()
Returns: layup active status Return type: bool New in version NX7.5.0.
License requirements: nx_lam_composites (“Laminate Composites”)
-------------------------------------
Setter Method
Signature
ActiveStatus(active)
Parameters: active (bool) – layup active status New in version NX7.5.0.
License requirements: nx_lam_composites (“Laminate Composites”)
FiberOrientationOptions¶
-
LaminateGlobalLayup.
FiberOrientationOptions
¶ Returns the fiber orientation options
-------------------------------------
Getter Method
Signature
FiberOrientationOptions()
Returns: the fiber orientation options Return type: NXOpen.CAE.LaminateFiberOrientationOptions
New in version NX7.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
IsOccurrence¶
-
LaminateGlobalLayup.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
LaminateGlobalLayup.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Label¶
-
LaminateGlobalLayup.
Label
¶ Returns or sets the global layup label
-------------------------------------
Getter Method
Signature
Label()
Returns: layup label Return type: int New in version NX7.5.0.
License requirements: nx_lam_composites (“Laminate Composites”)
-------------------------------------
Setter Method
Signature
Label(label)
Parameters: label (int) – layup label New in version NX7.5.0.
License requirements: nx_lam_composites (“Laminate Composites”)
Name¶
-
LaminateGlobalLayup.
Name
¶ Returns or sets the global layup name
-------------------------------------
Getter Method
Signature
Name()
Returns: layup name Return type: str New in version NX7.5.0.
License requirements: nx_lam_composites (“Laminate Composites”)
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – layup name New in version NX7.5.0.
License requirements: nx_lam_composites (“Laminate Composites”)
OwningComponent¶
-
LaminateGlobalLayup.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
LaminateGlobalLayup.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
LaminateGlobalLayup.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
StackingRecipe¶
-
LaminateGlobalLayup.
StackingRecipe
¶ Returns or sets the global layup stacking recipe
-------------------------------------
Getter Method
Signature
StackingRecipe()
Returns: stacking recipe Return type: NXOpen.CAE.LaminateGlobalLayupStackingRecipeType
New in version NX7.5.0.
License requirements: nx_lam_composites (“Laminate Composites”)
-------------------------------------
Setter Method
Signature
StackingRecipe(stacinkRecipe)
Parameters: stacinkRecipe ( NXOpen.CAE.LaminateGlobalLayupStackingRecipeType
) – stacking recipeNew in version NX7.5.0.
License requirements: nx_lam_composites (“Laminate Composites”)
PlyGroups¶
-
LaminateGlobalLayup.
PlyGroups
¶ The list of ply groups associated to global layup
Signature
PlyGroups()
New in version NX6.0.2.
Returns: Return type: NXOpen.CAE.LaminateGlobalLayupPlyGroupCollection
Method Detail¶
AutogroupByMaterials¶
-
LaminateGlobalLayup.
AutogroupByMaterials
¶ Create groups for materials
Signature
AutogroupByMaterials()
New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ClearLayup¶
-
LaminateGlobalLayup.
ClearLayup
¶ Removes all the ply groups and plies from the global layup
Signature
ClearLayup()
New in version NX7.5.0.
License requirements: nx_lam_composites (“Laminate Composites”)
CreateFiberOrientationOptionsBuilder¶
-
LaminateGlobalLayup.
CreateFiberOrientationOptionsBuilder
¶ Creates a
NXOpen.CAE.LaminateFiberOrientationOptionsBuilder
Signature
CreateFiberOrientationOptionsBuilder()
Returns: Return type: NXOpen.CAE.LaminateFiberOrientationOptionsBuilder
New in version NX7.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
CreateLockAngleBuilder¶
-
LaminateGlobalLayup.
CreateLockAngleBuilder
¶ Creates a
NXOpen.CAE.LaminateLockAngleBuilder
Signature
CreateLockAngleBuilder()
Returns: Return type: NXOpen.CAE.LaminateLockAngleBuilder
New in version NX7.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
DefineSymPlyidRange¶
-
LaminateGlobalLayup.
DefineSymPlyidRange
¶ Defines the range of id to be used for symmetric and repeated plies.
Signature
DefineSymPlyidRange(minId, maxId)
Parameters: - minId (int) – Minimum symmetric ply id, inclusive
- maxId (int) – Maximum symmetric ply id, exclusive
New in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
ExportDrapingDomainAsGroups¶
-
LaminateGlobalLayup.
ExportDrapingDomainAsGroups
¶ Exports draping domain to a group
Signature
ExportDrapingDomainAsGroups(individualPlyGroups)
Parameters: individualPlyGroups (bool) – If true, create one group per ply. If false, put everything in the same group New in version NX7.5.2.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ExportDrapingResults¶
-
LaminateGlobalLayup.
ExportDrapingResults
¶ Exports draping results to a csv file.
Signature
ExportDrapingResults(csvFilename, showShearAngle, showYarnAngle, showPrimaryDirection, showSecondaryDirection, showNormalDirection)
Parameters: - csvFilename (str) –
- showShearAngle (bool) –
- showYarnAngle (bool) –
- showPrimaryDirection (bool) –
- showSecondaryDirection (bool) –
- showNormalDirection (bool) –
New in version NX7.5.1.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ExportLayup¶
-
LaminateGlobalLayup.
ExportLayup
¶ Export simple layup definition to a csv file.
Corresponds to the CSV layup export button in the Ply Layup section of the Layup Modeler dialog.
Signature
ExportLayup(csvFilename)
Parameters: csvFilename (str) – New in version NX8.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ExportPliesToFibersim¶
-
LaminateGlobalLayup.
ExportPliesToFibersim
¶ Exports ply definitions to FiberSim using the hdf5 file format.
Signature
ExportPliesToFibersim(filename)
Parameters: filename (str) – File to which the plies will be exported using the FiberSim hdf5 format. New in version NX8.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
FindObject¶
-
LaminateGlobalLayup.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Information¶
-
LaminateGlobalLayup.
Information
¶ Display global layup information
Signature
Information(detailed)
Parameters: detailed (bool) – New in version NX7.5.1.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Print¶
-
LaminateGlobalLayup.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.