LaminateGlobalLayupStackingRecipeType Enumeration

NXOpen.CAE.LaminateGlobalLayup.StackingRecipeType is an alias for NXOpen.CAE.LaminateGlobalLayupStackingRecipeType

class NXOpen.CAE.LaminateGlobalLayupStackingRecipeType

Bases: object

Used to specify the stacking recipe of the global layup

Enum Members

Enum Member Enum Member Description
Normal
Normal
Symmetric
Symmetric
SymmetricWithCore
Symmetric with core
Repeated
Repeated
RepeatedWithCore
Repeated with core
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.