DurabilityTransientEventBuilder Class

class NXOpen.CAE.DurabilityTransientEventBuilder

Bases: NXOpen.CAE.DurabilityEventBuilder

Represents the builder for the transient durability event.

There is no kf creator for this.

New in version NX7.5.0.

Properties

Property Description
DataControl Returns the data control.
EventName Returns or sets the event name.
MdfFileName Returns or sets the mdfFileName.
ResultSourceTag Returns or sets the source of results for the event.
Sort2Access Returns or sets the sort2 access.
StaticOffset Returns or sets the static offset for the event.
Subcase Returns or sets the subcase index.
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
SetAxissearch The stress axes stored inside the event.
SetFatigue The event fatigue settings stored inside the event.
SetSolveoptions The event overrides.
SetStrength The event strength settings stored inside the event.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

DataControl

DurabilityTransientEventBuilder.DataControl

Returns the data control.

-------------------------------------

Getter Method

Signature DataControl()

Returns:
Return type:NXOpen.CAE.DurabilityDataControlBuilder

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

MdfFileName

DurabilityTransientEventBuilder.MdfFileName

Returns or sets the mdfFileName.

-------------------------------------

Getter Method

Signature MdfFileName()

Returns:
Return type:str

New in version NX8.0.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

-------------------------------------

Setter Method

Signature MdfFileName(filename)

Parameters:filename (str) –

New in version NX8.0.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

Sort2Access

DurabilityTransientEventBuilder.Sort2Access

Returns or sets the sort2 access.

-------------------------------------

Getter Method

Signature Sort2Access()

Returns:
Return type:bool

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Sort2Access(sort2Access)

Parameters:sort2Access (bool) –

New in version NX8.0.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

StaticOffset

DurabilityTransientEventBuilder.StaticOffset

Returns or sets the static offset for the event.

-------------------------------------

Getter Method

Signature StaticOffset()

Returns:
Return type:NXOpen.NXObject

New in version NX8.0.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

-------------------------------------

Setter Method

Signature StaticOffset(staticOffset)

Parameters:staticOffset (NXOpen.NXObject) –

New in version NX8.0.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

Subcase

DurabilityTransientEventBuilder.Subcase

Returns or sets the subcase index.

-------------------------------------

Getter Method

Signature Subcase()

Returns:
Return type:int

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

-------------------------------------

Setter Method

Signature Subcase(subcase)

Parameters:subcase (int) –

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

Method Detail

Validate

DurabilityTransientEventBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.