DurabilityEventBuilder Class

class NXOpen.CAE.DurabilityEventBuilder

Bases: NXOpen.Builder

Represents the abstract builder class for all durability events.

This is an abstract class, and cannot be created.

New in version NX7.5.0.

Properties

Property Description
EventName Returns or sets the event name.
ResultSourceTag Returns or sets the source of results for the event.
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
SetAxissearch The stress axes stored inside the event.
SetFatigue The event fatigue settings stored inside the event.
SetSolveoptions The event overrides.
SetStrength The event strength settings stored inside the event.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

EventName

DurabilityEventBuilder.EventName

Returns or sets the event name.

-------------------------------------

Getter Method

Signature EventName()

Returns:
Return type:str

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

-------------------------------------

Setter Method

Signature EventName(title)

Parameters:title (str) –

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

ResultSourceTag

DurabilityEventBuilder.ResultSourceTag

Returns or sets the source of results for the event.

-------------------------------------

Getter Method

Signature ResultSourceTag()

Returns:
Return type:NXOpen.NXObject

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

-------------------------------------

Setter Method

Signature ResultSourceTag(resultSourceTag)

Parameters:resultSourceTag (NXOpen.NXObject) –

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

Method Detail

SetAxissearch

DurabilityEventBuilder.SetAxissearch

The stress axes stored inside the event.

Signature SetAxissearch(axisSearch)

Parameters:axisSearch (NXOpen.CAE.DurabilityAxisSearch) –

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

SetFatigue

DurabilityEventBuilder.SetFatigue

The event fatigue settings stored inside the event.

Signature SetFatigue(fatigue)

Parameters:fatigue (NXOpen.CAE.DurabilityFatigue) –

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

SetSolveoptions

DurabilityEventBuilder.SetSolveoptions

The event overrides.

Signature SetSolveoptions(solveOption)

Parameters:solveOption (NXOpen.CAE.DurabilitySolveOptions) –

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

SetStrength

DurabilityEventBuilder.SetStrength

The event strength settings stored inside the event.

Signature SetStrength(strength)

Parameters:strength (NXOpen.CAE.DurabilityStrength) –

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

Validate

DurabilityEventBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.